HI Keita
with source modifications one can set any
frequency. However I would suggest to work with
default, as freescale BSP releases optimized with this frequency.
Best regards
igor
HI Keita
max. frequency is 333MHz according to Table 18-4. System Clock
Frequency Values i.MX6SDL Reference Manual (rev.2 5/2015),
it is not possible to set it to 352 MHz.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your quick response.
>it is not possible to set it to 352 MHz.
Is it possible to set the 333MHz in i.MX6DL with jb4.2.2?
Or, should one use the default VPU freq?
Best Regards,
Keita