About VPU @352MHz in i.MX6SDL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About VPU @352MHz in i.MX6SDL

Jump to solution
1,006 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have known that VPU frequency can set at 352 MHz in i.MX6DQ.

Is it possible to set 352 MHz in the i.MX6SDL, too?

If it is not possible, how much max frequency is it possible to set in i.MX6SDL?

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
792 Views
igorpadykov
NXP Employee
NXP Employee

HI Keita

with source modifications one can set any

frequency. However I would suggest to work with

default, as freescale BSP releases optimized with this frequency.

Best regards

igor

View solution in original post

0 Kudos
4 Replies
792 Views
igorpadykov
NXP Employee
NXP Employee

HI Keita

max. frequency is 333MHz according to Table 18-4. System Clock

Frequency Values i.MX6SDL Reference Manual (rev.2  5/2015),

it is not possible to set it to 352 MHz.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
792 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your quick response.

>it is not possible to set it to 352 MHz.

Is it possible to set the 333MHz in i.MX6DL with jb4.2.2?

Or, should one use the default VPU freq?

Best Regards,

Keita

0 Kudos
793 Views
igorpadykov
NXP Employee
NXP Employee

HI Keita

with source modifications one can set any

frequency. However I would suggest to work with

default, as freescale BSP releases optimized with this frequency.

Best regards

igor

0 Kudos
792 Views
keitanagashima
Senior Contributor I

Dear Igor,

Hello. Thank you very much!

OK. I got it.

Best Regards,

Keita

0 Kudos