Dear All,
Hello. I have a question about D_CAL and TXCAL45DP/DN in USBPHYx_TXn register.
Refer to attached file.
And, please answer to me.
I referred the below topic. But, I couldn't understand it.
Best Regards,
Keita
已解决! 转到解答。
HI Keita
please find attached file with answer.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Keita
please find attached file with answer.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Hello. Thank you for your quick reply.
In case of D_CAL=0000b, 1.19*17.78mA = 21.1582[mA].
But, the it was described Resistor trimming code = 0.16% in RM.
In case of D_CAL=1111b, 0.79*17.78mA = 14.0462[mA].
But, the it was described Resistor trimming code = +25% in RM.
How should I calculate it from RM?
(I didn't understand the relation of your value and RM one.)
Best Regards,
Keita
HI Keita
these resistors are for trimming the current, as described in AN4589
I do not think that you can calculate it from RM,
I provided you info from AE team (SR-2466611351), one can
just use it.
Best regards
igor