ADV7482 MIPI on imx6q board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADV7482 MIPI on imx6q board

1,115 Views
zky141225
Contributor II

bret @CarlosCasillas

   We are using ADV7482 on our board with iMX6Q and I am trying to modify ov5642_mipi.c for adv7482_mipi_tvin.c. I have two questions when I modified the driver.

   I use Bsp is L3.0.35_linux. 

when I try  ./mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 1024 -oh 768 -m 4 -bg

I hope to get your help.,thanks

Questions as follows

webwxgetmsgimg.jpg

wxgetmsgimg.jpg

this is log:

ERROR: unrecognized std! 59565955 (PAL=ff, NTSC=b000

RGB565
frame buffer width 1024, height 768, bytesperline 2048
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001

Labels (3)
0 Kudos
Reply
1 Reply

822 Views
joanxie
NXP TechSupport
NXP TechSupport

how about try to use mxc_v4l2_tvin.out? it seems de-interlacing issue

0 Kudos
Reply