Hello
I would like to improve my project.
If i have 4 x DDR3 chips on the same layer(top or bottom). From now i will call them "M" with a number.
May i crate an hybrid topology between T and fly-by using chip selects and multiple clocks?
Like
M1-M2 use CLK0 diff signal, CS0 data D[0-31]
&
M3-M4
use CLK1,CS1 and data D[32-63].
May i do that or i'm forced to use only first 32bits(data)?
The address lines could divide in 2 between 2 memory group like the T topology, like they are routed between M2 and M3 and then split.
.--------------MPU----------.
ck0 ||||addr ck1
|M1||M2| <=====> |M3||M4|
Hi Massimo
>May i crate an hybrid topology between T and fly-by using chip selects and multiple clocks?
sorry this is not recommended.
>M3-M4 use CLK1,CS1 and data D[32-63].
>May i do that or i'm forced to use only first 32bits(data)?
MMDC allows only first 32bits(data) as described in
sect.44.12.1 MMDC Core Control Register (MMDCx_MDCTL) for "DSIZ" field
i.MX 6Dual/6Quad Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------