Dear all,
Our customer would like to connect the camera which outputs a 16bit YUV422 data to CSI of i.MX6Solo.
However, this camera outputs data by the progressive 262.5H form.
Please see the following example.
Does CSI of i.MX6 support progressive 262.5H?
Best Regards,
Yuuki
Solved! Go to Solution.
Hi yuuki
supported formats are given in
sect.4.11.10.1 IPU Sensor Interface Signal Mapping IMX6DQCEC ,
sorry progressive 262.5H is not natively supported.
However it may be supported as 16 bits “generic-data” input.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki
supported formats are given in
sect.4.11.10.1 IPU Sensor Interface Signal Mapping IMX6DQCEC ,
sorry progressive 262.5H is not natively supported.
However it may be supported as 16 bits “generic-data” input.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor-san,
Thank you for your support.
In 16 bit "generic-data" input,
Can that receive 262H and 263H alternately?
Best Regards,
Yuuki
Hi yuuki
yes, but one will have to parse data in software.
263H nor 262H are not natively supported in IPU hardware.
Best regards
igor