16bit YUV422 progressive 262.5H input for i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16bit YUV422 progressive 262.5H input for i.MX6Solo

Jump to solution
828 Views
yuuki
Senior Contributor II

Dear all,

Our customer would like to connect the camera which outputs a 16bit YUV422 data to CSI of i.MX6Solo.

However, this camera outputs data by the progressive 262.5H form.

Please see the following example.

progressive 262.5H.png

Does CSI of i.MX6 support progressive 262.5H?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
660 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

supported formats are given in

sect.4.11.10.1 IPU Sensor Interface Signal Mapping IMX6DQCEC ,

sorry progressive 262.5H is not natively supported.

However it may be supported as 16 bits  “generic-data” input.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
661 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

supported formats are given in

sect.4.11.10.1 IPU Sensor Interface Signal Mapping IMX6DQCEC ,

sorry progressive 262.5H is not natively supported.

However it may be supported as 16 bits  “generic-data” input.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
660 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.


In 16 bit "generic-data" input,
Can that receive 262H and 263H alternately?

Best Regards,
Yuuki

0 Kudos
Reply
660 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes, but one will have to parse data in software.

263H nor 262H are not natively supported in IPU hardware.

Best regards

igor