Hi Freescale,
我们要基于i.MX28平台上来开发一款产品,想获取到i.MX28 的source code。Freescale
是通过ltib 来提供的source code ,我根据所提供的文档,在ubuntu14.04 desktop版上试图使用ltib来
获取到i.MX28 linux 和uboot的source code,可是在安装ltib时遇到了些麻烦(ltib实在是太麻烦了),
using /home/dany/ima28/L2.6.35_1.1.0_130130_source/litb_28/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: libtool
=====================
Processing: lkc
=================
Build path taken because: directory build, no prebuilt rpm,
Cowardly refusing to clobber existing directory:
/opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4
Remove this by hand if you really want to rebuild this package from scratch
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
Started: Fri Jan 30 14:21:23 2015
Ended: Fri Jan 30 14:21:28 2015
Elapsed: 5 seconds
These packages failed to build:
lkc
Build Failed
在build ltib时,会有以上的failed log,(rpm 有安装)
请帮忙看看是什么原因,
另外,我们项目进度的原因,请先帮忙提供下i.MX28 linux 和uboot的source code,
非常感谢!!
BR,
苏州佳世达电通有限公司
工业自动化部门
0512-66658800-6061
Hi 邓洲 邓
you can find below useful tips for building ltib
LTIB build fails on lkc, using Ubuntu 11.10 and LTIB 9.1.1
i.MX Linux BSP Environment Setup
https://community.freescale.com/docs/DOC-93454
https://community.freescale.com/docs/DOC-93455
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
thanks a lot,
According to your suggestion, I install the patches on my ubuntu14.04, use
./install-patches.sh <ltib full path>
show following failed info when build ltib,
"
Processing: elftosb
=====================
Build path taken because: no prebuilt rpm,
rpmbuild --dbpath ///opt/freescale/ltib/var/lib/rpm --target x86_64 --define '_unpackaged_files_terminate_build 0' --define '_target_cpu x86_64' --define '__strip strip' --define '_topdir /opt/freescale/ltib/usr/src/rpm' --define '_prefix /opt/freescale/ltib/usr' --define '_tmppath /home/dany/ima28/L2.6.35_1.1.0_130130_source/litb_28/ltib/tmp' --define '_rpmdir /opt/freescale/ltib/usr/src/rpm/RPMS' --define '_mandir /opt/freescale/ltib/usr/share/man' --define '_sysconfdir /opt/freescale/ltib/etc' --define '_localstatedir /var' -bb --clean --rmsource /home/dany/ima28/L2.6.35_1.1.0_130130_source/litb_28/ltib/dist/lfs-5.1/elftosb/elftosb.spec
error: Unable to open temp file.
Building target platforms: x86_64
Building for target x86_64
RPM build errors:
Unable to open temp file.
Build time for elftosb: 0 seconds
Failed building elftosb
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
Started: Thu Feb 5 16:47:30 2015
Ended: Thu Feb 5 16:47:31 2015
Elapsed: 1 seconds
These packages failed to build:
elftosb
Build Failed
"
error: Unable to open temp file. and use df command to check tmpfs, only 1% used
/dev/sda7 | 42301688 11638896 28490940 30% / | |||
none | 4 | 0 | 4 | 0% /sys/fs/cgroup |
udev | 1013364 | 4 1013360 | 1% /dev | |
tmpfs | 204896 | 1152 203744 | 1% /run | |
none | 5120 | 4 | 5116 | 1% /run/lock |
none | 1024476 | 76 1024400 | 1% /run/shm | |
none | 102400 | 68 102332 | 1% /run/user | |
/dev/sda1 | 48128436 22795268 25333168 48% /media/dany/AEB89C1FB89BE45D | |||
/dev/sdb1 | 14429008 6993592 7435416 49% /media/dany/UUI |
Are there any other method to get the i.MX28 linux and uboot source code?
thanks!!
BR
Dany
Hi Dany
suggest to install 9.04, ltib should be
built without problems on that release
http://old-releases.ubuntu.com/releases/9.04/
~igor
Hello,
I followed this https://community.freescale.com/docs/DOC-98910
And I can build in Ubuntu 14.04 64 bits
Luis