i.Mx6 CSI Test Mode Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx6 CSI Test Mode Question

i.Mx6 CSI Test Mode Question

The customer would like to test BT.656 using Test mode. Is it supported?

  1. 38.4.3.3 Test mode in RM shows only one CSIx_SENS_CONG setting. Does it mean Test mode support only one as follows?

Does Test mode support other settings?

CSIx_EXT_VSYNC = 0x1

CSIx_DATA_WIDTH = 0x1

CSIx_SENS_DATA_FORMAT = 0x0

CSIx_PACK_TIGHT = 0x0

CSIx_SENS_PRTCL = 0x1

CSIx_SENS_PIX_CLK_POL = 0x1

CSIx_DATA_POL = 0x0

CSIx_HSYNC_POL = 0x0

CSIx_VSYNC_POL = 0x0

For example,

customer want to know if Test mode support  CSIx_SENS_PRTCL=0x2or 0x3 instead of 0x1?

customer want to know if Test mode support CSIx_SENS_DATA_FORMAT=0x1or 0x2 instead of 0x0?

Answer:

CSI CM TEST MODE is working as below:

1,only ungated mode.

2,data width should be configured to 8

3,data format should be configured to rgb888

It cannot be other format such as bt656. It uses CSI1_TST_CTRL register to configure {R,G,B} 24 bit value and taking it as RGB888/YUV444 format for further process.  The generated image size is due to the configured width & height in the registers.

ラベル(4)
タグ(3)
評価なし
バージョン履歴
最終更新日:
‎06-06-2013 02:14 AM
更新者: