i.MX31 PDK Setting Buttons and Jumpers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX31 PDK Setting Buttons and Jumpers

i.MX31 PDK Setting Buttons and Jumpers

i.MX31 - 3 Stack

There are two boot modes for IMX31PDK. In Internal Boot mode, the processor will execute an address from internal memory, and in External Boot mode the processor will execute an address from a external memory properly configured. This modes can be configured setting the values of dip switch SW5-SW10 shown in image below.

400px-Imx31-3stack.png

Debug board. Top view.

External Boot from Flash

In this mode, the processor will execute an address into a external flash (NAND).

If there is a bootloader saved in the right place in flash, it will be executed and the system will start. If there are a kernel image and a root file system saved configured, the operational system will start.


External_boot.png


The values for the IMX31PDK dip switches programming the boot sequence are show in table below.

SW5 SW6 SW7SW8SW9SW10
Internal Boot (programming flash)000000
External Boot from Flash010000

Internal Boot

The Internal Boot mode enables ATK to communicate with processor and perform the writing of images into flash (bootloader image, kernel image and root file system image).

Internal_boot.png


評価なし
バージョン履歴
最終更新日:
‎08-22-2012 09:16 AM
更新者: