Source code you have is one week old now. So, first step is synchronize it.
$ repo sync
$ repo start <new branch name> --all
If you change *any* source code (for choosing another preferred kernel, for example) and want to sync again, or use master instead of dylan, you may be able to rebase or sync your source code, even with changes.
Or you found a bug, fixed that, and want to send a patch to community.
Example of a system with 2 branches: zeus and new_feature (the asterisk shows the current branch)
$ repo branches
* new_feature | in all projects
zeus | in all projects
The following command display the usage, with a list of all supported machines, all supported community distros and examples of Poky's distro:
$ source setup-environment build
Usage: MACHINE=<machine> DISTRO=<distro> source setup-environment <build-dir>
Usage: source setup-environment <build-dir>
<machine> machine name
<distro> distro name
<build-dir> build directory
The first usage is for creating a new build directory. In this case, the
script creates the build directory <build-dir>, configures it for the
specified <machine> and <distro>, and prepares the calling shell for running
bitbake on the build directory.
The second usage is for using an existing build directory. In this case,
the script prepares the calling shell for running bitbake on the build
directory <build-dir>. The build directory configuration is unchanged.
Supported machines:
apalis-imx6
ccimx6ulsbcexpress
ccimx6ulsbcpro
cgtqmx6
cm-fx6
colibri-imx6
colibri-imx6ull
colibri-imx7
colibri-vf
cubox-i
imx233-olinuxino-maxi
imx233-olinuxino-micro
imx233-olinuxino-mini
imx233-olinuxino-nano
imx6dl-riotboard
imx6qdl-variscite-som
imx6q-dms-ba16
imx6qsabrelite
imx6sl-warp
imx6ul-pico
imx7d-pico
imx7s-warp
m28evk
m53evk
nitrogen6sx
nitrogen6x
nitrogen6x-lite
nitrogen7
nitrogen8m
pcm052
tx6q-10x0
tx6q-11x0
tx6s-8034
tx6s-8035
tx6u-8033
tx6u-80x0
tx6u-81x0
ventana
wandboard
imx23evk
imx25pdk
imx28evk
imx51evk
imx53ard
imx53qsb
imx6qdlsabreauto
imx6qdlsabresd
imx6slevk
imx6sllevk
imx6sxsabreauto
imx6sxsabresd
imx6ulevk
imx6ullevk
imx7dsabresd
imx7ulpevk
imx8mmevk
imx8mqevk
imx8qmmek
imx8qxpmek
ls1012afrwy
ls1012ardb
ls1021atwr
ls1043ardb
ls1046ardb
ls1088ardb
ls1088ardb-pb
ls2080ardb
ls2088ardb
lx2160ardb
mpc8548cds
p1020rdb
p2020rdb
p2041rdb
p3041ds
p4080ds
p5040ds-64b
p5040ds
t1024rdb-64b
t1024rdb
t1042d4rdb-64b
t1042d4rdb
t2080rdb-64b
t2080rdb
t4240rdb-64b
t4240rdb
Supported Freescale's distros:
fslc-framebuffer
fslc-wayland
fslc-x11
fslc-xwayland
Available Poky's distros:
poky-altcfg
poky-bleeding
poky
poky-tiny
Examples:
- To create a new Yocto build directory:
$ MACHINE=imx6qdlsabresd DISTRO=fslc-framebuffer source setup-environment build
- To use an existing Yocto build directory:
$ source setup-environment build
ERROR: You must set MACHINE when creating a new build directory.
An example of command line to setup the build environment is (read and answer if you accept EULA or not):
MACHINE=imx8mmevk DISTRO=fslc-wayland source setup-environment build
(...)
Do you accept the EULA you just read? (y/n) y
EULA has been accepted.
Welcome to Freescale Community BSP
The Yocto Project has extensive documentation about OE including a
reference manual which can be found at:
http://yoctoproject.org/documentation
For more information about OpenEmbedded see their website:
http://www.openembedded.org/
You can now run 'bitbake <target>'
Common targets are:
core-image-minimal
meta-toolchain
meta-toolchain-sdk
adt-installer
meta-ide-support
Your build environment has been configured with:
MACHINE=imx8mmevk
SDKMACHINE=i686
DISTRO=fslc-wayland
EULA=
Now, you are in new created build directory.
Your default build/conf/local.conf file can looks like:
MACHINE ??= 'imx8mmevk'
DISTRO ?= 'fslc-wayland'
PACKAGE_CLASSES ?= 'package_rpm'
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-system-native = " sdl"
CONF_VERSION = "1"
DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"
For the current list of supported board, take a look on FSL Community BSP Release Notes 2.4 (Draft document) documentation
Or, see the FSL Community BSP Release Notes
There are a huge list of images available. Some images includes more packages than others, you can see a list of FSL Community BSP images with description here.
The list of supported images from Yocto Project (with description) is here.
When an image has more packages included, it takes longer to build.
Another way to list all the images you have installed in your metadata is:
$ find ../sources -name *image*
For the goal of this training, any image is good, but a suggestion is presented in next command line:
(make sure you are still in build directory)
$ cd build
$ bitbake core-image-base
Note (Sept2019): Required disk space for build image is ~31GB
Go to Yocto Training - HOME
My 2 cents:
1. It would be nice to point to the other non-freescale machines Yocto supports.
2. The biggest image is (I believe) fsl-image-gui-sdk, but from user's perspective the fsl-image-gui is the fattest (perhaps adding a footnote to indicate this)
3. The link to Task # 1 is missing at the end of the document
Daiane, let me know if you want me to include the above changes (if you first approve them :smileyhappy: )
Leo
I pointed to meta-fsl-arm release notes, but I can include the non-freescale board supported.
For fsl-image-gui/-sdk, I think it´s not the right task to point how both images diverges. I prefer to start with core-image-base and then include another task at the end showing a more complete "how to" for images, maybe how to create one image from scratch. What do you think?
Thanks a lot Leo :smileygrin:
hello,
the conf file for "imx6qsabrelite.conf" is not in this folder anymore.
I dont see it in the git folder or in my computer after the download.
github.com/Freescale/meta-fsl-arm
or
/fsl-community-bsp/build/conf
Where did it go ?
Thanks
ssinfo
What should be the value for the BB_NUMBER_THREAD and PARALLEL_MAKE for the sabrelite in the conf/local.conf file?
By default, the value are:
BB_NUMBER_THREADS = '1'
PARALLEL_MAKE = '-j 1'
Should I set the value to 4 or 8 ?
Thanks
I think I find the answer. It seems these two fields are related to bitbake settings for the host computers.
So it is not related to the target..
Source:
Yocto Project Reference Manual
Please correct me if I am wrong.
thanks
Hi
if you ran the setup-enviroment script, it automatically sets these for your. Both values should be equal to the number of cores on your HOST machine. You can also try doubling this value for the MAKE related variable, but I do not think you gain much.
Leo
The instructions above are very simple, but I seem to be getting a few problems, I'm afraid. I changed conf/local.conf to use "imx6qsabrelite" and ran bitbake.
I get a few warnings, which I'm guessing are OK since they seem to use mirror sites instead, but I'm also getting some errors which appear to be fatal, regarding the Boundary Devices git repository.
I tried accessing the Boundary Devices git repository without bitbake (just typing "git clone git://github.com/boundarydevices/linux-imx6.git") and that seems to work without any errors, so is it possible that there's a problem with bitbake somewhere?
All comments / suggestions welcome!
Full output is shown below:
dchirgwin@dc-ubuntu2:~/fsl-community-bsp/build$ bitbake core-image-base
Pseudo is not present but is required, building this first before the main build
Parsing recipes: 100% |#########################################| Time: 00:02:15
Parsing of 1277 .bb files complete (0 cached, 1277 parsed). 1645 targets, 68 skipped, 0 masked, 0 errors.
Build Configuration:
BB_VERSION = "1.18.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-12.10"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabrelite"
DISTRO = "poky"
DISTRO_VERSION = "1.4.2"
TUNE_FEATURES = "armv7a vfp neon"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "bct:d734ab491a30078d43dee5440c03acce2d251425"
meta-oe = "bct:81bf02c1ed858b8a7ae9297b8eab7d9355d0a48c"
meta-fsl-arm = "bct:afe2162644544a92a517f1d51211fdcb76bb1a29"
meta-fsl-arm-extra = "bct:5f5a9cfcad223f5a1c623346780510ffcdc012ab"
meta-fsl-demos = "bct:724cfb929748f47782dea3b1dc412b028f6f3515"
NOTE: Resolving any missing task queue dependencies
NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 63 tasks of which 0 didn't need to be rerun and all succeeded.
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 1646 entries from dependency cache.
Build Configuration:
BB_VERSION = "1.18.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-12.10"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabrelite"
DISTRO = "poky"
DISTRO_VERSION = "1.4.2"
TUNE_FEATURES = "armv7a vfp neon"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "bct:d734ab491a30078d43dee5440c03acce2d251425"
meta-oe = "bct:81bf02c1ed858b8a7ae9297b8eab7d9355d0a48c"
meta-fsl-arm = "bct:afe2162644544a92a517f1d51211fdcb76bb1a29"
meta-fsl-arm-extra = "bct:5f5a9cfcad223f5a1c623346780510ffcdc012ab"
meta-fsl-demos = "bct:724cfb929748f47782dea3b1dc412b028f6f3515"
NOTE: Resolving any missing task queue dependencies
NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL http://www.zlib.net/zlib-1.2.7.tar.bz2, attempting MIRRORS if available
WARNING: Failed to fetch URL ftp://ftp.ossp.org/pkg/lib/uuid/uuid-1.6.2.tar.gz, attempting MIRRORS if available
WARNING: Failed to fetch URL http://www.apache.org/dist/apr/apr-util-1.5.1.tar.gz, attempting MIRRORS if available
WARNING: Failed to fetch URL http://www.apache.org/dist/subversion/subversion-1.7.8.tar.bz2, attempting MIRRORS if available
WARNING: Failed to fetch URL git://github.com/boundarydevices/linux-imx6.git, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/dchirgwin/fsl-community-bsp/downloads//git2/github.com.boundarydevices.linux-imx6.git'...
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
ERROR: Function failed: Fetcher failure for URL: 'git://github.com/boundarydevices/linux-imx6.git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/dchirgwin/fsl-community-bsp/build/tmp/work/imx6qsabrelite-poky-linux-gnueabi/linux-boundary/3.0.35-r0/temp/log.do_fetch.7065
ERROR: Task 281 (/home/dchirgwin/fsl-community-bsp/sources/meta-fsl-arm-extra/recipes-kernel/linux/linux-boundary_3.0.35.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 983 tasks of which 148 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/dchirgwin/fsl-community-bsp/sources/meta-fsl-arm-extra/recipes-kernel/linux/linux-boundary_3.0.35.bb, do_fetch
Summary: There were 5 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
dchirgwin@dc-ubuntu2:~/fsl-community-b
are you able to download those packages if you use wget?
$ wget ftp://ftp.ossp.org/pkg/lib/uuid/uuid-1.6.2.tar.gz
for example?
I can use wget for the FTP link, but all three HTTP links fail with 404 using wget.
Taking the subversion link as an example, if I go to the parent directory http://www.apache.org/dist/subversion I can see that the required file (version 1.7.8) is not actually there - the oldest version seems to be 1.7.11.
Well,
When I face the downloads issues I wait for sometime and try again.
You can try to get the same package from other source.
Hi Daiane,
Thanks for the response. I just modified my post a few minutes ago with new information, which you may not have seen:
Taking the subversion link as an example, if I go to the parent directory http://www.apache.org/dist/subversion I can see that the required file (version 1.7.8) is not actually there - the oldest version seems to be 1.7.11.
Does that make a difference?
Regards,
Dave C
I'm getting a bit further with this now. The packages I can't load are not actually present on the relevant web sites, because they have been superseded.
http://www.zlib.net/zlib-1.2.7.tar.bz2 has been replaced with 1.2.8
http://www.apache.org/dist/apr/apr-util-1.5.1.tar.gz has been replaced with 1.5.2
http://www.apache.org/dist/subversion/subversion-1.7.8.tar.bz2 has been replaced with 1.7.11
The "master" branch in yocto poky has already made the necessary changes to use the new packages instead, but the "dylan" branch has not. I tried changing the repo manifest to use the "master" branch instead, but that causes other problems. I guess the answer is to push the necessary changes to yocto and then everyone can get them.
Any comments?
From yocto point of view, yes, it makes all difference. Yocto only "see" the right version package, because it only "looks for" the right version package.
But, if you think you can use another version, you can change the recipe in order to "add a new package".
I don´t think it worth. Be sure your Internet connection is OK. Be sure all mirrors are up. And try again. Yesterday I was able to go from download source code from a complete image downloading everything again. So I think it was only a period of instability.
Thanks for the material!
It works fine on my 64-bit Ubuntu 12.04 with i5 processor but fails on my 32-bit Ubuntu 12.04 with qual-core processor.
But something strange happens while giving 'bitbake core-image-base'.
It automatically shuts down my system everytime. I have not copied anything betwenn my two machines.
I need to work only on my 32-bit system. Can you please help??
muthuswamydikshit, without more context (as build log or something) it is hard to guess.
My rough guess is not enough memory for the build and/or disk space. Yocto is voracious for computational resources so this might be the cause of problem.
I have a Intel dual-core 1.93Ghz(I guess) processor.
More than 200GB hard disk space and 3GB RAM.
OS: Ubuntu 12.04 LTS (32-bit)
I dint have application running while building.
Is this not sufficient ?
Moreover, I was compiling only for a base image not gui.
It automatically shuts down every time.
Under build/tmp/work, I can find only 3 files.
Any hints to overcome this problem?
From your description it seems to be a hardware issue; I'd bet a fan issue.
Hi all,
in dylan branch I think there is a bug in file:
/build/tmp/work/i686-linux/elfutils-native/0.148-r11/line2addr.c
at line 135 there is: switch (sscanf (a.arg, "%a[^:]:%d", &a.file, &a.line))
instead of: switch (sscanf (a.arg, "%m[^:]:%d", &a.file, &a.line))
This bug causes a compilation error when I try:
bitbake fsl-image-test
In master branch I don't found the same issue, but in this branch there isn't the memtool!
Please verify!
Bye.
P.S.: the compilation error is:
| /media/francesco/DATI/yocto-bsp/build/tmp/work/i686-linux/elfutils-native/0.148-r11/elfutils-0.148/tests/line2addr.c:135:7: error: format '%a' expects argument of type 'float *', but argument 3 has type 'char **' [-Werror=format=]
| switch (sscanf (a.arg, "%a[^:]:%d", &a.file, &a.line))
| ^
Hi francpalm (there are three francesco Palmisanos on the community, is that you multiple times?!!) Tthanks for sharing the fix. This patch does not belong to meta-fsl-* layers (I think), so it must be send to another list.
Before you send the patch, can you rebuilt your image with an new build folder? if case you have already done this, ignore this step and send the patch.
OtavioSalvador FYI.
Leo
Thanks for letting us know!
You really need to be on dylan, now that dora was released? In this case we can work together to get it fixed on your local files. I would need to double check if dylan is still supported for bugfixes..... :smileysad:
Dylan is still being maintained; it just needs to be send as a fix for oe-core mailing list.
Please put:
[for-dylan][PATCH] ...
in subject for the patch. So people handle it accordingly.
Hi all,
for LeonardoSandovalGonzalez : I don't know the other two my omonymous! I changed my avatar in a car (I work on automotive projects :-D )!
I've already deleted all my files and repeated the Daiane guide with dylan and with master branch. Master branch don't have the issue.
for DaianeAngolini : if you suggest to use dora I'll be happy to follow your advice. The image fsl-image-test has the memtool already installed?
for OtavioSalvador : I'm a beginner in this world but I'll be happy to learn how create and send a patch. I don't want to mess!
If you have some time to help me I thanks in advance.
Bye.
I can help, for sure.
Please try to reproduce your issue with dora branches and if you do, please get a patch applied in Poky to fix it.
Once you does it, I can help with the upstreaming process for it :-)
My memory is not trustable at all. I remember memtool was already installed on fsl-image-test at some point of time. When? I don´t know.
But add on your local.conf:
CORE_IMAGE_EXTRA_INSTALL += "memtool"
and you will have it installed on *any* image (much better than rely on my memory :D)