Q&A: How is VPU Latency on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Q&A: How is VPU Latency on i.MX6

Q&A: How is VPU Latency on i.MX6

Q: What is latency figures for the VPU to decode

Device: i.MX6Q

OS: Linux
Resolution:                         1920x1080(HD)

Frame rate:                        30 FPS

Function:                             Overlay messages.

Input/Output:                   8 bit / YUV 4:2:0 / NAL stream

Profile level:                      4.1. Constrained Baseline. I and P frames support.

A:

It depend on the syntax in H.264, includes num_reorder_frames,max_dec_frame_buffering,num_ref_frames,MaxDpbSize,etc. for start latency: it cover vpu driver loading, allocate buffers, init, decoding the first frame less than 100ms on iMX6/Linux.

This document was generated from the following discussion: VPU Latency i.MX6

ラベル(2)
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎09-01-2013 11:22 PM
更新者: