PICO-PI-IMX7 support in upstream projects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PICO-PI-IMX7 support in upstream projects

PICO-PI-IMX7 support in upstream projects

The PICO-PI-IMX7 is a TechNexion board defined here. It is now supported in mainline U-Boot, mainline Kernel, FSL Community BSP and Buildroot.

In mainline U-Boot it is supported since v2017.07.

In mainline Linux Kernel it is supported since 4.13.

To generate an image for PICO-PI-IMX7 using FSL Community BSP, please see: The imx7d-pico board is now supported in FSL Community BSP - i.MXDev Blog.
To generate an image for PICO-PI-IMX7 using Buildroot, please see: The imx7d-pico board is now supported in Buildroot - i.MXDev Blog.

标签 (3)
无评分
版本历史
最后更新:
‎10-03-2017 05:49 AM
更新人: