This document provides the steps to patch and build a fastboot Linux System. This document assumes the BSP 3.0.35_1.1.0 and a i.MX6Q platform. For more information about what the patches do, please check this link.
u-boot:
Prepare u-boot source code (./ltib -m prep -p u-boot)
Move to u-boot folder (cd rpm/BUILD/u-boot-2009.08)
Download u-boot attached patches
Patch code (for p in *.patch; do patch -p1 < $p;done)
kernel:
Prepare kernel source code (./ltib -m prep -p kernel)
Move to kernel folder (cd rpm/BUILD/linux)
Download attached kernel patches
Patch code (for p in *.patch; do patch -p1 < $p;done)
Could you please attach patches for SabreAI board??
Unfortunately I do not have them. You may need to patch manually. In case you do this, please share your sabre AI patches.
Leo
Hi,Why i can't find "imx6_ssd_lite_defconfig" in "arch/arm/configs" ? my device is imx6q.
Have you got these files for MarS Board (embest-tech)?
And Have you got full image (not just patch)?
which version of u-boot is used? uboot-2009.08?? There is no file/folder named mx6qsabresd in this version of u-boot!
How much time u_boot takes to finish in milisecs?