Following docs(English or Chinese version) are also can be referred as a hand on guide.
Freescale i.MX6 DRAM Port Application Guide-DDR3
Please find i.Mx6DQSDL LPDDR2 Script Aid through below link.
Please find i.Mx6DQSDL DDR3 Script Aid through below link.
Please find i.MX6SX DDR3 Script Aid through below link..
Any questions are welcome!
Change History:
0.02 - Add total 1Gbit density supporting.
Is there a newer version of the file? I saw a presentation with 5 tabs and also ARM DS-5 support... (https://community.nxp.com/docs/DOC-331528 )
Thanks! hkr
Hello LinWang,
Greetings of the day...
We have a customized imx6ul board which is having the two RAM chips(MT41K512M8DA-107P) connected parallel and using one CS pin DRAM_CS0. is this script support to test the 1GB DDR stress and calibration? where can i find the 1GB density script.
Thanks & Regards
Ganesh.K