linux recovery mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linux recovery mode

2,702 Views
yoonseok
Contributor III

 

in a Linux environment

I want to restore images such as linux images and rootfilesystem in recovery mod like Android.

Please teach me the way.

0 Kudos
Reply
2 Replies

2,696 Views
BiyongSUN
NXP Employee
NXP Employee

You can try u-boot  boot count mechanism. 

It gets nothing to do any chip, it is pure software.

The  basic idea is similar to android.

 

 

SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK

SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK - NXP Community

 

SWUpdate OTA i.MX8MM EVK_rev3.pdf

 

无标题.png

 

0 Kudos
Reply

2,697 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello yoonseok.

The recovery mode is a feature for Android only, there is no such recovery mode for Linux. 

By the way, which product are you working with it? 

 

Best regards

Harvey

0 Kudos
Reply