we are testing thread stack using test harness. the USB-KW41Z is used as sniffer.
but we have a mistake that we downloade a KW24D512 firmware into USB-KW41Z through SWD KW41Z interface. and changed the bootloader.
now the test harness can not recognize the USB-KW41Z as sniffer.
how to revert to default firmware?
thanks.
Hello Fei,
In order to flash an image to the USB-KW41Z, you need to have a Segger J-Link programmer (which I presume you have, given that you managed to flash a wrong image).
You can flash it with Test Tool, the image is already there, see the picture below.
Tell me if it's ok.
Regards,
Lilian
Thank you for your response.
I have flashed the sniffer_usbkw41z_k22f.bin, but the it is still not OK.
I guess the reason that the wrong bootloader is reprogrammed, checked "Browse bootloader file" in last process.
Would we flash the bootloader again? If so, where is the file?
Thank you very much.
Hello Fei,
Are you sure that Thread Harness worked before with USB-KW41Z? The NXP sniffer used for harness is USB-KW24. The firmware for it you can find in [...]/Firmwares/NXP(Freescale)/Sniffer folder, in the folder in which you have installed Thread Harness.
Regards,
Lilian
Yes, Thread Harness supports both USB-KW41Z and USB-KW24D512, and all certification labs must use USB-KW41Z from 2018 according to Thread Group policy. So we purchased USB-KW41Z. All USB-KW41Z device are OK before refrash.
Thank you very much.
It works very well after I update this firmware.