Zigbee 3.0: short address bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee 3.0: short address bug

322 Views
Janson
Contributor I

Hello every one:
       Using the Zigbee 3.0 code example with the JN5169 chip, the short address of the router program changes autonomously after a period of use. What conditions trigger the change in the short address? After the short address changes, there is no notification sent to the Zigbee node bridge about the new short address, resulting in the inability to control it.

0 Kudos
Reply
1 Reply

269 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Janson

Hope you are doing well.

Please, consider that JN5189/88T is preferred for any new Zigbee design.

Could you please help us with more details about your setup? What is the Application Note you used as base for your development?

Have you modified the base source code? If so, what are the modifications you added?

Can you share a sniffer log from your tests?

Any additional information is greatly appreciated.

Regards,
Eduardo.

0 Kudos
Reply