What is the active equivalent to the nt3h2111?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the active equivalent to the nt3h2111?

707件の閲覧回数
hrj
Contributor I

What is the active equivalent to the nt3h2111?

I need a chip that can initiate the communication and generate the 13.56MHz carrierwave

I need to communicate with a device with a NT3H2111 chip on it, så that it is correctly configured when we ship the device.

What  would you recommend?

Regards

Henrik

 

0 件の賞賛
返信
2 返答(返信)

692件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One may refer to NTAG 5 link to replace NTAG I2C.

URL:https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-tags-for-electronics/ntag-5-link-nfc-forum-complian....

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

664件の閲覧回数
hrj
Contributor I

Hi

Thank you for your response, but i think you misunderstood my question

I do not need a replacement chip. I need a chip that can act as a MASTER in the nfc communication with the NT3H2111

I need a chip that can initiate the communication eg. act as the telehone side of the NFC communication, as we need to configure the devices we produced before we deliver them. Using a phone to configure them individually is too tedious

Regards

Henrik

 

0 件の賞賛
返信