What drivers to use to download to the USB-KW24D512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What drivers to use to download to the USB-KW24D512?

ソリューションへジャンプ
1,380件の閲覧回数
smachin
Contributor II

Hi All,

I am trying to get some of the Thread code examples working with my USB-KW24D512.  I am using IAR & Windows 7.  The projects build fine, but when I go to download to the target the compiler brings up the dialog show in the screenshot below.  What additional steps are needed to get this to work?

kinetis debug screenshot.png

0 件の賞賛
返信
1 解決策
1,083件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Sean,

You have to use external debugger such as JLink and P&E's Multilinks(Universal and Universal FX).

Cheers,

Antonio

元の投稿で解決策を見る

3 返答(返信)
1,083件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Sen,

Not the first time.

Please have a look at the below link for the USB MSD Bootloader:

https://community.nxp.com/docs/DOC-102539

Cheers,

Antonio

0 件の賞賛
返信
1,084件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Sean,

You have to use external debugger such as JLink and P&E's Multilinks(Universal and Universal FX).

Cheers,

Antonio

1,083件の閲覧回数
smachin
Contributor II

I see.  There is absolutely no way to flash the device over USB?