What drivers to use to download to the USB-KW24D512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What drivers to use to download to the USB-KW24D512?

Jump to solution
1,380 Views
smachin
Contributor II

Hi All,

I am trying to get some of the Thread code examples working with my USB-KW24D512.  I am using IAR & Windows 7.  The projects build fine, but when I go to download to the target the compiler brings up the dialog show in the screenshot below.  What additional steps are needed to get this to work?

kinetis debug screenshot.png

0 Kudos
Reply
1 Solution
1,083 Views
antonioconcio
NXP Employee
NXP Employee

Hi Sean,

You have to use external debugger such as JLink and P&E's Multilinks(Universal and Universal FX).

Cheers,

Antonio

View solution in original post

3 Replies
1,083 Views
antonioconcio
NXP Employee
NXP Employee

Hi Sen,

Not the first time.

Please have a look at the below link for the USB MSD Bootloader:

https://community.nxp.com/docs/DOC-102539

Cheers,

Antonio

0 Kudos
Reply
1,084 Views
antonioconcio
NXP Employee
NXP Employee

Hi Sean,

You have to use external debugger such as JLink and P&E's Multilinks(Universal and Universal FX).

Cheers,

Antonio

1,083 Views
smachin
Contributor II

I see.  There is absolutely no way to flash the device over USB?