I am trying to bring up a custom board using a SJA1105s and I cannot get any traffic to go through the system.
Architecture:
Software Info:
My Findings:
Linux believes it is sending data out of the system and TX packet counters will increment, there are no RX packets. However I am not seeing any information data out of the system. I have probed both the RX and TX lines on the PHY and can see RX data coming in (data into the switch) but no data on the TX line (Data leaving the switch). I do not have acsess to the RX/TX lines between CPU and SJA to see what is happening there.
The SJA1105 driver recognizes the PHY as a 88E1510, the same family but without SGMII. Looking at the Marvell driver it seems to indicate they are the same software wise.
The SJA1105 driver does notify when the Ethernet cord is removed/replugged, so it appears it is monitoring the PHY.
My Concerns/Problems:
edit:
The driver sets the host port to 1 which is connected to the CPU.
The SJA1105 driver sets the host port to port 0, all implementations seem to have port 0 be the port connected to the CPU. My design does not, is this an issue? Can it be solved with a change to the device tree or something in the driver? Does this require a board revision to debug?
The driver marks all untagged packets to be dropped. Does this mean I need to configure a VLAN system with tagging on the CPU? I attempted to follow the startup scripts used by LS1021A-TSN-RD. I did not notice any info about VLAN tagging.
Thank you in advance,
Let me know if you need anymore information from me.
The connections look like this:
┌──────────────────────────────┐
│ │
│ │
│ │
│ │
│ │
│ ┌───────────┴───────────────┐
│ │ SPI │
┌─────▼─────────┐ │ │
│ SPI │ │ │
│ │ │M │
│ 1◄────────┤A │
│ SJA1105 │ │C │
│ │ │ CPU │
│ │ │ ATSAMA5d36 │
│ │ │ │
│ 0 │ │ │
└───────┬───────┘ │ │
│ │ MDIO │
│ └──────────┬────────────────┘
│ │
│ │
│ │
┌─────────▼────────┐ │
│ RGMII │ │
│ │ │
│ PHY │ │
│ 88E1512 M│ │
│ D◄──────────────────┘
│ I│
│ O│
│ │
└───────┬──────────┘
│
│
│
│
│
│
│
│
│
└► OUT
The device tree:
&macb0 {
phy-mode = "rgmii-id";
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
status = "okay";
fixed-link {
speed = <1000>;
full-duplex;
};
mdio{
#address-cells = <1>;
#size-cells = <0>;
t1phy0: ethernet-phy@0{//may not need the driver specified
compatible = "ethernet-phy-ieee802.3-c22", "marvell,88e1512";
reg = <0x0>;
};
};
};
&spi0 {//Ethernet Switch
pinctrl-names = "default", "cs";
pinctrl-1 = <&pinctrl_spi0_cs>;
cs-gpios = <&pioD 13 0>;
status = "okay";
//5 port switch
sja1105@0 {
compatible = "nxp,sja1105s";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0>;
spi-max-frequency = <44000000>;//44MHz
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
//specify for spi mode 1
//spi-cpol;//cpol not needed
spi-cpha;//shifted clock phase
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {//Ethernet out
reg = <0>;
label = "lan1";
phy-handle = <&t1phy0>;
phy-mode = "rgmii-id";
};
port@1 {//MAC
label = "cpuMAC";
phy-mode = "rgmii-id";
reg = <1>;
ethernet = <&macb0>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
};
Solved! Go to Solution.
Here is the log. The issue is the log seems to indicate the switch is up and is active. However, no packets can be sent through the switch. I am not seeing any data pass out of lan1 nor do I see any traffic in linux (eth0).
atmel_spi: Using dma0chan4 (tx) and dma0chan5 (rx) for DMA transfers
sja1105@0 enforce active low on chipselect handle
sja1105 spi0.0: Probed switch chip: SJA1105S
sja1105 spi0.0: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
sja1105 spi0.0: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
macb ethernet eth0: Cadence GEM rev 0x00020119 at 0xf0028000 irq 30 (02:10:a0:94:77:20)sja1105 spi0.0: Probed switch chip: SJA1105S
sja1105 spi0.0: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
sja1105 spi0.0: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
sja1105 spi0.0: configuring for fixed/rgmii-id link mode
sja1105 spi0.0: Link is Up - 1Gbps/Full - flow control off
sja1105 spi0.0 lan1 (uninitialized): PHY [f0028000.ethernet-ffffffff:00] driver [Marvell 88E1510] (irq=POLL)
device eth0 entered promiscuous modeDSA: tree 0 setup
Starting network: macb f0028000.ethernet eth0: configuring for fixed/rgmii link mode
macb f0028000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
OK
sja1105 spi0.0 lan1: configuring for phy/rgmii-id link mode
sja1105 spi0.0 lan2: configuring for fixed/rgmii-id link mode
sja1105 spi0.0 lan2: Link is Up - 1Gbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): lan2: link becomes ready
sja1105 spi0.0 lan3: configuring for fixed/rgmii-id link mode
sja1105 spi0.0 lan3: Link is Up - 1Gbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): lan3: link becomes ready
write 1 to vlan_filtering to enable VLAN filtering
br0: port 1(lan1) entered blocking state
br0: port 1(lan1) entered disabled state
device lan1 entered promiscuous mode
br0: port 2(lan2) entered blocking state
br0: port 2(lan2) entered disabled state
device lan2 entered promiscuous mode
br0: port 3(lan3) entered blocking state
br0: port 3(lan3) entered disabled state
device lan3 entered promiscuous mode
br0: port 3(lan3) entered blocking state
br0: port 3(lan3) entered forwarding state
br0: port 2(lan2) entered blocking state
br0: port 2(lan2) entered forwarding statesja1105 spi0.0 lan1: Link is Up - 1Gbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): lan1: link becomes ready
br0: port 1(lan1) entered blocking state
br0: port 1(lan1) entered forwarding state
Hello @mtcastle,
Apologies for the delayed response
Just to let you know that I am still working on your questions, I will let you know as soon as I have an update.
Thank you so much for your patience
Regards,
Sebastian
Hello @mtcastle,
I would like to inform you that I'm working on your question, I will let you know as soon as I have an update.
Thank you so much for your patience
Regards,
Sebastian