QN9090/9030 Mesh

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9090/9030 Mesh

Jump to solution
2,182 Views
Nxpfan
Contributor I

Hi Does QN9090/QN9030 sdk support ble mesh? If yes, then how to get demo and lib? If no, does NXP have plan to support ble mesh in QN9090/9030 sdk?

Thanks,

0 Kudos
Reply
1 Solution
2,128 Views
nxf56274
NXP Employee
NXP Employee

Hi,

We have not developed the zigbee sdk. So it can only used the ble. If you want to use mesh network, we recommend the K32W061.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
2,164 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The QN9090 ble can connect to up to 16 device at the same time in theory. But it is not convenient to organize the network compared with zigbee. And we do not have the sdk to realize the multiple connection.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,154 Views
Nxpfan
Contributor I

Hi TIC,

Thanks for reply. From nxp post: https://media.nxp.com/news-releases/news-release-details/nxp-delivers-new-bluetooth-microcontroller-...

it states QN serials has ble support. Does it mean NXP have plan to support ble mesh sdk?

Does any other nxp product support ble mesh?

Thanks,

Tags (1)
0 Kudos
Reply
2,145 Views
nxf56274
NXP Employee
NXP Employee

Hi,

mesh network (or simply meshnet) is a local network topology in which the infrastructure nodes (i.e. bridges, switches, and other infrastructure devices) connect directly, dynamically and non-hierarchically to as many other nodes as possible and cooperate with one another to efficiently route data from/to clients. The ble do not support. The qn9090 support the 802.15.4 that the zigbee rely on. So the zigbee is more suitable to support the mesh network.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,136 Views
Nxpfan
Contributor I

Hi TIC,

ok, then  BLE mesh(or bluetooth SIG mesh) is not supported on QN9090/9030 SDK. You mentioned "The qn9090 support the 802.15.4 that the zigbee rely on" , so does QN9090 SDK  support zigbee feature already or is there any document about qn9090 zigbee information?

 

Thanks,

0 Kudos
Reply
2,129 Views
nxf56274
NXP Employee
NXP Employee

Hi,

We have not developed the zigbee sdk. So it can only used the ble. If you want to use mesh network, we recommend the K32W061.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply