Hi
Thanks
已解决! 转到解答。
Hi Sen,
1. The stack implements version 1.1.1 of the Thread Group core specification. The Thread stack has been certified by Thread Group. The are no plans to implement other Thread versions into the KW41Z platform, only maintenance.
2. Not within the KW41Z stack, that'd need to be taken cared of in the host processor. ie. k64+cr20a or external linux host
3. Just in the external host
Hi Sen,
1)See Kinetis MKW2xD and MCR20A Connectivity Software
2) No, we currently just support FSCI for host serial communication.
Hi Sen,
Linux already supports NAT64 and IPv4 and you'd have the TAP tunnel in place.
You could also take a look into the K64+CR20A Thread topology as reference which I believe it also has nat64.
Thanks jcpacheco,
1) Where can I see the code for K64+CR20A Thread topology? I could not find any documentation.
2) Does NXP support OTBR - spinel protocol implementation? I see only FSCI interface in the SDK.
https://openthread.io/guides/ncp/
https://github.com/openthread/ot-br-posix
Hi Sen,
1. The stack implements version 1.1.1 of the Thread Group core specification. The Thread stack has been certified by Thread Group. The are no plans to implement other Thread versions into the KW41Z platform, only maintenance.
2. Not within the KW41Z stack, that'd need to be taken cared of in the host processor. ie. k64+cr20a or external linux host
3. Just in the external host