NCx3340 can not detected multiple end point card T1T (Topaz512)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NCx3340 can not detected multiple end point card T1T (Topaz512)

488 次查看
robokuta02
Contributor I

I'm using S32K144 evb-Q100 board and NCX3340 add on board. I'm testing with multiple endpoint. When I put 2 card T1T (Topaz-512) into the RF field and send discovery command. The NFCC didn't response correctly with information provide in user manual (UCAI-1402 user manual page 130). The correct way is NFCC should response RF_DISCOVER_NTF before send RF_INTF_ACTIVATED_NTF but I didn't get command RF_DISCOVER_NTF.

So, could everyone ever meet this problem? I noticed that: I had checked with card T2T and it's working correctly. Thank you so much.

 

robokuta02_0-1627541062801.png

 

0 项奖励
回复
1 回复

471 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

NCx3340 is for automotive market, while our services are for mass market, so we don't have info regarding this product. Sorry for the inconvenience may cause.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励
回复