I am writing a Client Application based on Temperature_collector example. On the Server side I have a custom BLE Service. With pairing disabled, the Client application can discover the Services on the Server and read Characteristic data. But when I enable Pairing, I see that Gap_Pair(peerDeviceId, &gPairingParameters) request is sent, but I do not receive a 'gConnEvtPairingResponse_c' in the ble_conn_manager.c. After some time I receive a HCI Connection timeout. Am I missing something here?
Client Side Pairing parameters:
解決済! 解決策の投稿を見る。
Hi,
We were finally able to root cause the issue. The issue was due to a watchdog timer in our code. The BLE_APP task was taking more than 40ms during pairing operation. This was happening when SecLib code was executed on the request of the BLE Host stack. Since the watchdog task could not get a chance to execute it would reset the system, causing HCI timeout on the other device.
This was a little tricky to debug because if a debugger is connected then the watchdog gets disabled and the issue was not seen.
Your suggestion of running the code in EVM helped us during root causing the issue.
We have now moved the BLE App task to execute in the background so that the Watchdog can interrupt it. And now pairing works fine.
Thanks a lot for your support.
Hi,
Do you enable the 'gAppUseBonding_d' in file 'app_preinclude.h'?
Prepare a phone that can scan the ble. When your service broadcast, use your phone to try to pair. Does your phone pop out the window like this?
If so, I think that the problem may happens to client.
Please also refer the chapter 4.1.3 and 4.2.2 in attachment.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thank you for your response.
Hi,
I use ble_shell example. I add this code in connection callback to test if the client can receive the gConnEvtPairingResponse_c when pair.
The result shows that the client can receive the 'gConnEvtPairingResponse_c'.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks again for your response.
In my example I am waiting until the pairing is complete to even search for primary services. Do you think that can have an impact?
In your shell example that you executed was pairing done right after Connection establishment, before any GATT interactions are initiated?
Hi,
Before doing the service discovery, I do the paring.
Actually, If you try other paring examples, they always ignore this case 'gConnEvtPairingResponse_c'. So I think we do not need to check 'gConnEvtPairingResponse_c'.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
So if pairing is working before Service discovery in your case that means Pairing has no dependency on any GATT operation.
As for ignoring the 'gConnEvtPairingResponse_c', I specifically do not need this event, since I do not intend to take any action on it. But as soon as I start pairing I get HCI connection timeout. This is my main issue.
And as per the "Bluetooth Low Energy Application Developer's Guide.pdf", after the Pairing request from the Central, Pairing response is expected. So I suspect something is happening inside the Stack code that causes it to generate HCI timeout. Is there any debugging mechanism to further root cause the issue?
Hi,
How do you get the information about timeout? Which function returns this information? Show some code.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Print every event we receive in here. Let's check the connection sequence. And check which event is handled by mcu before time out.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Following is the sequence of events on the hardware in the order they are received:
ConnectionCallBack events in Central:
gConnEvtConnected_c
gConnEvtSlaveSecurityRequest_c
gConnEvtLeDataLengthChanged_c
(after a gap of few seconds)
gConnEvtDisconnected_c (with reason HCI Connection Timeout)
ConnectionCallBack events In Peripheral:
gConnEvtConnected_c
gConnEvtPairingRequest_c
gConnEvtLeDataLengthChanged_c
(after a gap of few seconds)
gConnEvtDisconnected_c (with reason HCI Connection Timeout)
Also attached is the ble_conn_manager.c file that takes care of the pairing procedure. Same file is used in both peripheral and Central.
Hi,
Central
pConnectionEvent ->:0 gConnEvtConnected_c
Connected!
pConnectionEvent ->:2 gConnEvtSlaveSecurityRequest_c
pConnectionEvent ->:19 gConnEvtLeDataLengthChanged_c
pConnectionEvent ->:3 gConnEvtPairingResponse_c
pConnectionEvent ->:27 gConnEvtPairingAlreadyStarted_c
pConnectionEvent ->:5 gConnEvtPasskeyRequest_c
pConnectionEvent ->:11 gConnEvtEncryptionChanged_c
pConnectionEvent ->:9 gConnEvtKeysReceived_c
pConnectionEvent ->:8 gConnEvtKeyExchangeRequest_c
pConnectionEvent ->:12 gConnEvtPairingComplete_c
Peripheral
pConnectionEvent ->:0 gConnEvtConnected_c
Connected!
pConnectionEvent ->:1 gConnEvtPairingRequest_c
pConnectionEvent ->:19 gConnEvtLeDataLengthChanged_c
pConnectionEvent ->:7 gConnEvtPasskeyDisplay_c
pConnectionEvent ->:11 gConnEvtEncryptionChanged_c
pConnectionEvent ->:8 gConnEvtKeyExchangeRequest_c
pConnectionEvent ->:9 gConnEvtKeysReceived_c
pConnectionEvent ->:12 gConnEvtPairingComplete_c
This is the normal process.
You stopped at gConnEvtLeDataLengthChanged_c. But this case doesn't handled by mcu. So the problem may happens to the before message. Please debug the peripheral function 'Gap_AcceptPairingRequest', check if it accepts the paring request. The hci timeout is because after the 'gConnEvtLeDataLengthChanged_c', the master and slave doesn't send info to each other.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
To make sure that the AcceptPairing function works fine, I have handled the error case as below in ble_conn_mgr.c:
//(void)Gap_AcceptPairingRequest(peerDeviceId, &gPairingParameters);
bleResult_t res = Gap_AcceptPairingRequest(peerDeviceId, &gPairingParameters);
if (gBleSuccess_c != res)
{
panic(0, 0, 0, 0);
}
Additionally I put a break point at this function to make sure it is executed and I see that the functions returns with success. So that means that either the Peripheral stack did not process the AcceptPairingRequest() properly or the Central Stack did not process the Pairing response sent by the Peripheral. Sadly I do not have a Sniffer tool to capture what is happening over the air. Do you have any suggestions on what could be going wrong. For your information this is my SDK version "SDK_2.6.11_FRDM-KW38". Earlier we were using the "2.6.6" version on which this issue was originally observed and hence we upgraded to "2.6.11".
Sincerely appreciating your support here.
Hi,
Do another test. Use the example 'temperature_collector ' without any modification. Use it to connect and bind. Does it work?
You need to modify the client scan callback. It will check if the scanned device has temperature profile. If your device doesn't contain, it won't connect to device. If your device doesn't contain the temperature profile, you would better comment this code. Use other way like device name to find specified device.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for the suggestion. It might take me a day or two to try this out but I will come back with the results.
Thanks and Regards,
Jeftha
HI,
We were able to get our hands on the KW38 eval board. So I will use the temperature_collector example and will put my code in the "temperature_collector.c" and will check the results. Will let you know how it goes.
Regards,
Jeftha
With the KW38 Eval board (with MCUXpresso IDE) acting as the Central and our Custom hardware working as the Peripheral we see the same observation.
Is it possible to get logs of the Stack in MCUXpresso IDE for EVB to see what is going on inside?
You'd better buy a ble sniffer. Analyzing the packet is more efficient.
The ble lib is invisible to us. So it's hard to get the information. The last way to try to find out the problem is using the Test tool. Use another board flashed with the fsci_black_box. The test tool provides the hci interface and it has the log about the hci commander.
Use this to control the device acting as the central. And check the log. This may help us.
Hi,
We were finally able to root cause the issue. The issue was due to a watchdog timer in our code. The BLE_APP task was taking more than 40ms during pairing operation. This was happening when SecLib code was executed on the request of the BLE Host stack. Since the watchdog task could not get a chance to execute it would reset the system, causing HCI timeout on the other device.
This was a little tricky to debug because if a debugger is connected then the watchdog gets disabled and the issue was not seen.
Your suggestion of running the code in EVM helped us during root causing the issue.
We have now moved the BLE App task to execute in the background so that the Watchdog can interrupt it. And now pairing works fine.
Thanks a lot for your support.