I want to read the firmware from MCU(JN5168)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to read the firmware from MCU(JN5168)

1,022 Views
hby9516
Contributor I

Hi. I'm using several industrial sensors, and I want to divide a group between the sensors, so I want to change the channel of one group. The MCU of this product uses JN5168, and the manufacturer doesn't provide a separate channel change method. Is there a way to check the firmware on the MCU or change the zigbee channel?

Labels (3)
0 Kudos
Reply
1 Reply

1,013 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Sorry, it can't be realized.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply