HW: i.mx8mm or i.mx8mp, + AW-CM358 (88w8987) or Murata 1YM (88W8997)
SW: SDK 6.6.3
WiFi:
Tried NXP EVK board
i.mx8mm
PCIE8997--16.92.21.p119.2-MM6X16437.p3-GPL-(FP92)
SD8987----16.92.21.p119.2-MM6X16437.p3-GPL-(FP92)
Customer side:
i.mx8mp kernel: 5.x
SD8997 ---- 16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL
Ref version:
Tried
i.mx8mm 6.1.22
SD8987----16.92.21.p76.5-MM5X16391.p3-GPL-(FP92)
PCIE8997--16.92.21.p84.4-MM5X16391.p3-GPL-(FP92)
No issue on this version.
Steps:
1. Convert conf to txpower bin by (refer to UM11490)
./mlanutl mlan0 hostcmd txpwrlimit_cfg_8987.conf generate_raw
txpower.bin
or
./mlanutl mlan0 hostcmd txpwrlimit_cfg_8997.conf generate_raw
txpower.bin
OK: without this line: txpwrlimit_cfg=nxp/txpower.bin
NOK(FW crash just after load txpower.bin): add this line txpwrlimit_cfg=nxp/txpower.bin
in /lib/firmware/nxp/wifi_mod_para.conf
and then bring up by
modprobe moal mod_para=nxp/wifi_mod_para.conf
FW crash after dmesg
txpwrlimit_cfg=nxp/txpower.bin
Logs share:
NOK logs:
663_p1192_8987_fail.txt
663_p1192_8997_fail.txt
OK logs:
663_p1192_8987_ok_noPwr.txt
663_p1192_8997_ok_noPwr.txt
6122_i.mx8mm_8987.txt
6122_p844_i.mx8mm_8997_noPwr_ok.txt
6122_p844_i.mx8mm_8997_withPwr_ok.txt
Customer can share their logs if needed.
Please help check if the procedure need to be changed after p119.2
Thanks.
解決済! 解決策の投稿を見る。
Hi, @yao_feng
I received our internal team feedback as below:
The reported issue is a regression issue and it is fixed already.
We have verified the changes on our local setup and it is working fine.
The release with the fixes will be available in Q2 (end of June).
Please help to update this info to our end customer and request them to verify on the Q2 release.
Thanks.
Best regards,
Christine.
Hi, @yao_feng
We are able to observe FW crash/Kernel panic as below on our local setup:
Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...
kernel: Internal error: Oops: 0000000096000007 [#1] PREEMPT SMP
Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...
kernel: Code: 91000f9c 1100077b 6b1b029f 54001a0b (38401743)
[ 244.448042] Timeout cmd id (244.444015) ??? [0xecf], act = 0x0
We are checking internally for further debugging the issue. We will update you soon.
Best regards,
Christine.
Hi, @yao_feng
I received our internal team feedback as below:
The reported issue is a regression issue and it is fixed already.
We have verified the changes on our local setup and it is working fine.
The release with the fixes will be available in Q2 (end of June).
Please help to update this info to our end customer and request them to verify on the Q2 release.
Thanks.
Best regards,
Christine.
Thanks for your reply.
Could you tell us when the new firmware will be available? 6/28?
Nancy
Hi, @NancyHuang
We have standalone release completed and available on the nxp.com with secure sign in.
Can you please check if this link can be accessible to you for the Q2 release?
Below link is for 88W8987:
Below link is for 88W8997:
Generic_SD-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL
Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL
If this is not accessible, then you may need to use Q2 (end of June) release available via i.MX BSP or Github release.
Thanks,
Christine.
Add more info.
if set
ps_mode=2
auto_ds=2
Got same result.