Hi,
We are using JN5179 as Zigbee Coordinator for our Product. We have designed a High Power module by taking the reference design of JN5179 M16 Module of DK5 and made few changes in DIO to configure the SKYWORKS chip.
We are facing issues while executing Customer Evaluation Tool (JN-AN-1210 - JN517x Customer Module Evaluation Tool). Various readings like RSSI is observed properly on M16 module while the same tests give wrong RSSI results on our production module.
We assume, these issues might be due to changes in DIOs made for our design as shown below.
*** Following are the changes made in our design which are different than the M16 DK5 design.
=================================================================
=================================================================
If DIO change is the issue then can you please provide the customer evaluation tool with above changes.
Hello,
The JN5179 it's not supported for mass market, could you please contact your sales representative for more information about this product?
Also, please consider that the support is limited for the JN5179.
Best Regards,
Estephania