Commissioning of Thread devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Commissioning of Thread devices

1,713 次查看
mihaidragnea
NXP Employee
NXP Employee

Thread uses a secure scheme of commissioning based on the proven DTLS open standard.

Users can authorize devices onto a Thread network using smart phones, tablets, or laptops/PCs. Also, GUI rich devices within the network can be used to authorize other devices.

When a new device is about to be enrolled in a Thread network, a security session is established between the new device and the commissioning device to authenticate and to provide the required credentials.

A Thread device can still function without a link to the internet provided by a Border Router. It can communicate with any other Thread device in the network or within the extended in-premise network.

标签 (1)
0 回复数