Hi,
I try to build JN-AN-1244 Dimmable Light under MCUXpresso IDE. First, I had a problem with the SDK path, which seems to be fixed now; however, when the build process starts it’s getting stuck at 20% and doesn’t move a bit. In the task manager, I see that ZPSConfig is working intensely but I have no clue what can be the problem.
Mariusz
Hi,
Please click the button 'detail' and make the screenshots. I want to check it. And what mcu you use?
When it stuck, does the build console goes on showing something?
Does your tool chain installed completely?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------