AFT09MS015NT1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AFT09MS015NT1

1,796 次查看
赵壮钦
Contributor II

_0-1676028936788.png

HELLO!

Our company purchased this model AFT09MS015NT1. After testing, we found these two problems. How can we solve them?

Attached is the test report

0 项奖励
回复
3 回复数

1,786 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Are you using any of our reference designs? Anyway, please check the Application note: RF LDMOS Optimum Biasing Circuit
https://www.nxp.com/docs/en/application-note/AN1643.pdf

Hope it helps.

0 项奖励
回复

1,743 次查看
赵壮钦
Contributor II

你好!

Thank you very much,We are not using biasing method described in NXP AN1643.pdf. That method is not the optimum for TETRA application (Pout +36dBm, Temperature -20 to +55degC, Vdd 10.8 to 15.6V).

Did you use the 046 in the same application as the 052 ( the part that was working properly)? - Yes both were used in same application and also tried on the same board (replacing one with another and only one of them worked)

0 项奖励
回复

1,740 次查看
赵壮钦
Contributor II

HELLO!

The attached pictures are as follows

0 项奖励
回复