The KW45 UART is overrun when more than 8 bytes are received.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The KW45 UART is overrun when more than 8 bytes are received.

305 Views
chenyu1
Contributor I

We have transplanted the reference code of UART interrupt, and use UART to receive data. If the serial port tool of the upper computer sends more than 8 bytes at a time, the following data will not be received, and if more than 8 bytes are overrun, please kindly help to check the problem, thank you!
The original KW45 lpuart_interrupt_transfer routine is fine to test, but will be overrun after porting more than 8 bytes.

a21a4e92-4fd6-4ae0-863d-76003ab38346.jpg

Labels (1)
  • KW

0 Kudos
1 Reply

284 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @chenyu1

Hope you are doing well.

I apologize for the inconvenience this might cause you, but this product has not been released yet. Could you please contact the person that provided you this board?

Regards,
Eduardo.

0 Kudos