The latest driver download for 88W9098 is p149: PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p149.8-17.26.1.p149.8-MXM5X17405_P4_V0V1-GPL.zip
When I extract this package, there doesn't seem to be a tarball that yields muart_src.
When I look at the p136: PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p136.54-17.26.1.p136.54-MXM5X17366_P30_V0V1-GPL.zip
It has a tarball UART-U16-X86-17.26.1.p136-2.2-M3X14100-GPL-src.tgz, which yields muart_src. Such tarball is not found from p149 download.
Is this an oversight in p149 packaging? Or is the muart source going to be delivered in some other download going forward.
Solved! Go to Solution.
Dear @CupOfTea
NXP has taken decision stop providing UART driver. Customer shall use the UART driver from Linux kernel (open source) itself.
Regards,
Olivier
Dear @CupOfTea
NXP has taken decision stop providing UART driver. Customer shall use the UART driver from Linux kernel (open source) itself.
Regards,
Olivier