The FW I'm using is:
SD-WLAN-UART-BT-8987-U16-MMC-W16.88.10.p72-16.26.10.p72-C4X16673-MGPL
Q1. Does the above FW support the following CVE?
CVE-2017-13081
CVE-2017-13080
CVE-2017-13079
CVE-2017-13078
CVE-2017-13077
Q2.If it is not supported, please tell me the supported FW version.
I asked a question on the case portal but got no response.
So I ask the community.
Hello,
I apologize for the delay, please help us check the EB - Marvell Wireless - WPA2 Vulnerability Update v2_10 , you can find it in the page fo the device. Please in case you do not see it shown, help us requesting higher access in the web page.
Regards
Dear Estephania,
thank you.
It could be confirmed. this case is closed
Best regards,
Sumi Kenji