88W8887 WIFI firmware download is failing during Firmware active check phase which running on IMX8DX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

88W8887 WIFI firmware download is failing during Firmware active check phase which running on IMX8DX

1,628 次查看
afridi20
Contributor III

88W8887 WIFI firmware download is failing during Firmware active check phase which running on IMX8DX

Hi,

I am trying to load the sd8887_wlan_a2.bin into Wifi driver. Initially, Firmware image download is completed without any issues. While moving into the Firmware activity check phase we are getting a firmwarestat flag as 0xf005 instead of 0xfedc.

Android version used:

1)Android Q10.0.0_2.6.0 (Linux 5.4.70 kernel)

Images and sources used:

1)SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p32-15.100.19.p32-C4X15647_A2-GPL

2)vendor_hal_007

Also, attached the log below for reference. Kindly help on this issue. Thank you in advance.

BOOT LOG:

[ 3.408213] si476x-core 18-0063: 18-0063 supply vd not found, using dummy regulator
[ 3.420244] si476x-core 18-0063: 18-0063 supply va not found, using dummy regulator
[ 3.429115] si476x-core 18-0063: 18-0063 supply vio1 not found, using dummy regulator
[ 3.440135] si476x-core 18-0063: 18-0063 supply vio2 not found, using dummy regulator
[ 3.449080] si476x-core 18-0063: No IRQ number specified, will use polling
[ 3.459093] si476x-core 18-0063: Error while sending command 0x11
[ 3.472640] si476x-core 18-0063: Error while sending command 0x01
[ 3.479796] si476x-core 18-0063: Power up failure(err = -5)
[ 3.488520] si476x-core 18-0063: Error while sending command 0x12
[ 3.489554] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.502478] i2c i2c-18: LPI2C adapter registered
[ 3.520242] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 3.542686] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12
[ 3.579228] mmc0: CQHCI version 5.10
[ 3.585395] pps pps0: new PPS source ptp0
[ 3.596829] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 3.603689] fec 5b040000.ethernet: Using random MAC address: 46:ac:bd:72:0c:e8
[ 3.613038] libphy: fec_enet_mii_bus: probed
[ 3.621695] fec 5b040000.ethernet eth0: registered PHC device 0
[ 3.666334] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.672997] [drm] No driver support for vblank timestamp query.
[ 3.679178] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.688017] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.695867] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.705354] imx-rproc imx8x_cm4@0: failed to find syscon
[ 3.710906] imx-rproc imx8x_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[ 3.720235] imx-rproc imx8x_cm4@0: No txdb, ret 0
[ 3.725920] remoteproc remoteproc0: imx-rproc is available
[ 3.760285] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 3.835403] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 3.893334] asoc-simple-card sound-bt-sco: bt-sco-pcm-wb <-> 59040000.sai mapping ok
[ 3.901165] asoc-simple-card sound-bt-sco: ASoC: no DMI vendor name!
[ 3.911921] i2c i2c-19: LPI2C adapter registered
[ 4.963692] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.991836] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.020001] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.048131] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.076194] ILITEK ERR line = 425 ilitek_i2c_write_and_read : ilitek_i2c_write_and_read, i2c write error, ret = -5
[ 5.092572] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.120614] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.148769] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.176956] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 5.204962] ILITEK ERR line = 432 ilitek_i2c_write_and_read : ilitek_i2c_write_and_read, i2c read error, ret = -5
[ 5.215440] ILITEK ERR line = 1804 ilitek_main_probe : init read tp protocol error so exit
[ 5.223928] ILITEK ERR line = 1877 ilitek_main_probe : return -ENODEV
[ 5.230681] i2c i2c-20: LPI2C adapter registered
[ 5.237220] mmc0: CQHCI version 5.10
[ 5.240908] sdhci-esdhc-imx 5b010000.mmc: allocated mmc-pwrseq
[ 5.590752] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 5.600613] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 5.607281] [drm] No driver support for vblank timestamp query.
[ 5.613320] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 5.622118]
[ 5.626833] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 5.634067]
[ 5.639063] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 5.647097] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[ 5.655684] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 5.664067] imx-drm display-subsystem: bound 56248000.dsi_host (ops nwl_dsi_component_ops)
[ 5.672376]
[ 5.676322]
[ 5.680661] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 5.793107]
[ 5.805550] Console: switching to colour frame buffer device 128x37
[ 5.812941]
[ 5.815583] mmc0: new high speed SDIO card at address 0001
[ 5.881700] imx-drm display-subsystem: fb0: imx-drmdrmfb frame buffer device
[ 5.898424] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 5.908348] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 5.920269] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 5.927021] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 5.935717] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 5.968029] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 5.974669] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 5.981223] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 5.988154] mx8-img-md: Unregistered all entities
[ 5.994878] ALSA device list:
[ 5.997921] #0: imx-audmix
[ 6.000833] #1: bt-sco-audio
[ 6.006551] Freeing unused kernel memory: 4416K
[ 6.020163] Run /init as init process
[ 6.074559] init: init first stage started!
[ 6.079230] init: Switching root to '/first_stage_ramdisk'
[ 6.088283] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 6.150820] init: [libfs_mgr]Created logical partition system_a on device /dev/block/dm-0
[ 6.160430] init: [libfs_mgr]Created logical partition system_b on device /dev/block/dm-1
[ 6.169760] init: [libfs_mgr]Created logical partition vendor_a on device /dev/block/dm-2
[ 6.179117] init: [libfs_mgr]Created logical partition vendor_b on device /dev/block/dm-3
[ 6.188458] init: [libfs_mgr]Created logical partition product_a on device /dev/block/dm-4
[ 6.197924] init: [libfs_mgr]Created logical partition product_b on device /dev/block/dm-5
[ 6.220426] init: [libfs_avb]Returning avb_handle with status: Success
[ 6.233335] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 6.254689] EXT4-fs (dm-6): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 6.283976] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 6.304565] EXT4-fs (dm-7): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 6.318169] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 6.343355] EXT4-fs (dm-8): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 6.400751] printk: init: 16 output lines suppressed due to ratelimiting
[ 6.432130] random: init: uninitialized urandom read (40 bytes read)
[ 6.702917] random: init: uninitialized urandom read (40 bytes read)
[ 6.742574] init: Loading SELinux policy
[ 6.806691] SELinux: Permission nlmsg_readpriv in class netlink_route_socket not defined in policy.
[ 6.816525] SELinux: the above unknown classes and permissions will be denied
[ 6.823796] SELinux: policy capability network_peer_controls=1
[ 6.829758] SELinux: policy capability open_perms=1
[ 6.834746] SELinux: policy capability extended_socket_class=1
[ 6.840845] SELinux: policy capability always_check_network=0
[ 6.846714] SELinux: policy capability cgroup_seclabel=0
[ 6.852156] SELinux: policy capability nnp_nosuid_transition=1
[ 6.998879] audit: type=1403 audit(13.172:2): auid=4294967295 ses=4294967295 lsm=selinux res=1
[ 6.999194] selinux: SELinux: Loaded policy from /vendor/etc/selinux/precompiled_sepolicy
[ 6.999194]
[ 7.018474] audit: type=1404 audit(13.192:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295 enabled=1 old-enabled=1 lsm=selinux res=1
[ 7.057191] selinux: SELinux: Loaded file_contexts
[ 7.057191]
[ 7.073801] random: init: uninitialized urandom read (40 bytes read)
[ 7.143211] init: init second stage started!
[ 7.199814] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 7.216951] selinux: SELinux: Loaded file_contexts
[ 7.216951]
[ 7.223403] init: Running restorecon...
[ 7.260381] init: Overriding previous 'ro.' property 'pm.dexopt.boot':'verify' with new value 'quicken'
[ 7.275780] init: Couldn't load property file '/product_services/build.prop': open() failed: No such file or directory: No such file or directory
[ 7.288986] init: Couldn't load property file '/factory/factory.prop': open() failed: No such file or directory: No such file or directory
[ 7.305074] init: Setting product property ro.product.brand to 'Android' (from ro.product.product.brand)
[ 7.314663] init: Setting product property ro.product.device to 'mek_8q' (from ro.product.product.device)
[ 7.324377] init: Setting product property ro.product.manufacturer to 'freescale' (from ro.product.product.manufacturer)
[ 7.452288] urandom_read: 4 callbacks suppressed
[ 7.452297] random: init: uninitialized urandom read (40 bytes read)
[ 7.537241] random: ueventd: uninitialized urandom read (40 bytes read)
[ 7.549062] random: apexd: uninitialized urandom read (40 bytes read)
[ 7.612254] ueventd: ueventd started!
[ 7.622323] selinux: SELinux: Loaded file_contexts
[ 7.622323]
[ 7.629064] ueventd: Parsing file /ueventd.rc...
[ 7.639750] ueventd: Parsing file /vendor/ueventd.rc...
[ 7.648556] ueventd: Parsing file /odm/ueventd.rc...
[ 7.653715] ueventd: Unable to read config file '/odm/ueventd.rc': open() failed: No such file or directory
[ 7.663655] ueventd: Parsing file /ueventd.freescale.rc...
[ 7.665166] apexd: Bootstrap subcommand detected
[ 7.669249] ueventd: Unable to read config file '/ueventd.freescale.rc': open() failed: No such file or directory
[ 8.100707] ueventd: firmware: loading 'regulatory.db' for '/devices/platform/regulatory.0/firmware/regulatory.db'
[ 8.132590] ueventd: loading /devices/platform/regulatory.0/firmware/regulatory.db took 32ms
[ 8.173941] apexd: wait for '/dev/loop-control' took 452ms
[ 8.180298] apexd: Pre-allocated 9 loopback devices
[ 8.192691] apexd: Scanning /system/apex for embedded keys
[ 8.212697] apexd: Scanning /product/apex for embedded keys
[ 8.228407] apexd: ... does not exist. Skipping
[ 8.233197] apexd: Scanning /system/apex looking for APEX packages.
[ 8.246185] apexd: Found /system/apex/com.android.media.apex
[ 8.253103] apexd: Skipped when bootstrapping
[ 8.257670] apexd: Found /system/apex/com.android.conscrypt.apex
[ 8.347329] EXT4-fs (loop0): mounted filesystem without journal. Opts: (null)
[ 8.427156] EXT4-fs (loop1): mounted filesystem without journal. Opts: (null)
[ 8.442462] printk: apexd: 13 output lines suppressed due to ratelimiting
[ 8.558380] Registered swp emulation handler
[ 8.642162] Console: switching to colour dummy device 80x25
[ 8.719393] watchdogd: watchdogd started (interval 10, margin 20)!
[ 8.778100] logd.auditd: start
[ 8.788100] logd.klogd: 8635980500
[ 8.796716] EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: discard
[ 8.942917] HCI UART driver ver 2.2-M2614100
[ 8.943005] HCI H4 protocol initialized
[ 8.960061] HCI BCSP protocol initialized
[ 8.969897] HCILL protocol initialized
[ 9.058298] sd8xxx: unknown parameter 'wakelock_timeout' ignored
[ 9.065874] wlan: Loading MWLAN driver
[ 9.077237] vendor=0x02DF device=0x9135 class=0 function=1
[ 9.083435] SDIO: max_segs=128 max_seg_size=65535
[ 9.088551] rx_work=1 cpu_num=2
[ 9.092863] wlan: Enable TX SG mode
[ 9.096974] wlan: Enable RX SG mode
[ 9.112181] Request firmware: nxp/sd8887_wlan_a2.bin
[ 9.134142] TP1 wlan_check_fw_status && POLL NO = 1
[ 9.139648]
[ 9.231767] zram0: detected capacity change from 0 to 629145600
[ 9.246951] TP3 wlan_check_fw_status && POLL NO = 1
[ 9.303200] mkswap: Swapspace size: 614396k, UUID=39a1533e-0745-49b1-b685-a8d5ce2b7fa0
[ 9.328053] Adding 614396k swap on /dev/block/zram0. Priority:-2 extents:1 across:614396k SS
[ 9.481289] random: crng init done
[ 9.599241] type=1400 audit(15.772:4): avc: denied { search } for comm="android.hardwar" name="/" dev="mmcblk1p6" ino=2 scontext=u:r:hal_bootctl_default:s0 tcontext=u:object_r:met0
[ 9.634707] type=1400 audit(15.772:4): avc: denied { search } for comm="android.hardwar" name="/" dev="mmcblk1p6" ino=2 scontext=u:r:hal_bootctl_default:s0 tcontext=u:object_r:met0
[ 9.654079] type=1400 audit(15.808:5): avc: denied { create } for comm="kdevtmpfs" name="dm-9" scontext=u:r:kernel:s0 tcontext=u:object_r:device:s0 tclass=blk_file permissive=0
[ 9.742233] Wlan: FW download over, firmwarelen=399832 downloaded 399832
[ 9.748996] wlan_check_fw_status && POLL NO = 100
[ 9.754591] wlan_sdio_read_fw_status
[ 9.861408] wlan_sdio_read_fw_status
[ 9.868264] tune2fs: tune2fs 1.44.4 (18-Aug-2018)
[ 9.868264]
[ 9.878817] EXT4-fs (dm-9): Ignoring removed nomblk_io_submit option
[ 9.896063] EXT4-fs (dm-9): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
[ 9.968464] wlan_sdio_read_fw_status
[ 10.075438] wlan_sdio_read_fw_status
[ 10.135566] e2fsck: e2fsck 1.44.4 (18-Aug-2018)
[ 10.135566]
[ 10.141929] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[ 10.141929]
[ 10.149615] e2fsck: Pass 2: Checking directory structure
[ 10.149615]
[ 10.156711] e2fsck: Pass 3: Checking directory connectivity
[ 10.156711]
[ 10.163946] e2fsck: Pass 4: Checking reference counts
[ 10.163946]
[ 10.170629] e2fsck: Pass 5: Checking group summary information
[ 10.170629]
[ 10.178145] e2fsck: userdata: 11/383520 files (0.0% non-contiguous), 46450/1531904 blocks
[ 10.178145]
[ 10.187984] TP3 wlan_sdio_read_fw_status
[ 10.275812] tune2fs: tune2fs 1.44.4 (18-Aug-2018)
[ 10.275812]
[ 10.295143] TP3 wlan_sdio_read_fw_status
[ 10.367165] EXT4-fs (dm-9): Ignoring removed nomblk_io_submit option
[ 10.383122] EXT4-fs (dm-9): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
[ 10.402663] TP3 wlan_sdio_read_fw_status
[ 10.452638] device-mapper: bow: Switching to state Checkpoint
[ 10.510899] TP3 wlan_sdio_read_fw_status
[ 10.617902] TP3 wlan_sdio_read_fw_status
[ 10.724894] TP3 wlan_sdio_read_fw_status
[ 10.831957] TP3 wlan_sdio_read_fw_status
[ 10.938918] TP3 wlan_sdio_read_fw_status
[ 11.045909] TP3 wlan_sdio_read_fw_status
[ 11.152917] TP3 wlan_sdio_read_fw_status
[ 11.259946] TP3 wlan_sdio_read_fw_status
[ 11.283439] init (pid 1) is setting deprecated v1 encryption policy; recommend upgrading to v2.
[ 11.364836] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
[ 11.366979] TP3 wlan_sdio_read_fw_status
[ 11.478948] TP3 wlan_sdio_read_fw_status
[ 11.570285] apexd: Marking APEXd as starting
[ 11.575500] fscrypt: AES-256-XTS using implementation "xts-aes-ce"
[ 11.583708] apexd: Scanning /system/apex for embedded keys
[ 11.586448] TP3 wlan_sdio_read_fw_status
[ 11.605970] apexd: Scanning /product/apex for embedded keys
[ 11.694343] EXT4-fs (loop2): mounted filesystem without journal. Opts: (null)
[ 11.696426] TP3 wlan_sdio_read_fw_status
[ 11.771117] EXT4-fs (loop3): mounted filesystem without journal. Opts: (null)
[ 11.808821] TP3 wlan_sdio_read_fw_status
[ 11.847196] EXT4-fs (loop4): mounted filesystem without journal. Opts: (null)
[ 11.915852] TP3 wlan_sdio_read_fw_status
[ 11.926207] EXT4-fs (loop5): mounted filesystem without journal. Opts: (null)
[ 12.004680] EXT4-fs (loop6): mounted filesystem without journal. Opts: (null)
[ 12.022809] TP3 wlan_sdio_read_fw_status
[ 12.083299] EXT4-fs (loop7): mounted filesystem without journal. Opts: (null)
[ 12.129613] TP3 wlan_sdio_read_fw_status
[ 12.167242] EXT4-fs (loop8): mounted filesystem without journal. Opts: (null)
[ 12.236334] TP3 wlan_sdio_read_fw_status
[ 12.343334] TP3 wlan_sdio_read_fw_status
[ 12.450298] TP3 wlan_sdio_read_fw_status
[ 12.557159] TP3 wlan_sdio_read_fw_status
[ 12.664080] TP3 wlan_sdio_read_fw_status
[ 12.771111] TP3 wlan_sdio_read_fw_status
[ 12.878115] TP3 wlan_sdio_read_fw_status
[ 12.985125] TP3 wlan_sdio_read_fw_status
[ 13.092110] TP3 wlan_sdio_read_fw_status
[ 13.199150] TP3 wlan_sdio_read_fw_status
[ 13.231853] init: Setting policy on /data/local
[ 13.236723] init: Policy for /data/local set to 0a70ce35fb6e87ec modes 1/4
[ 13.244059] init: Command 'mkdir /data/local 0751 root root' action=post-fs-data (/init.rc:500) took 1589ms and succeeded
[ 13.270719] init: Not setting policy on /data/preloads
[ 13.277316] init: Setting policy on /data/vendor
[ 13.282277] init: Policy for /data/vendor set to 0a70ce35fb6e87ec modes 1/4
[ 13.290450] init: Not setting policy on /data/vendor_ce
[ 13.296925] init: Not setting policy on /data/vendor_de
[ 13.306669] init: Not setting policy on /data/data
[ 13.311092] TP3 wlan_sdio_read_fw_status
[ 13.312936] init: Setting policy on /data/app-private
[ 13.418555] TP3 wlan_sdio_read_fw_status
[ 13.525560] TP3 wlan_sdio_read_fw_status
[ 13.632548] TP3 wlan_sdio_read_fw_status
[ 13.739552] TP3 wlan_sdio_read_fw_status
[ 13.846562] TP3 wlan_sdio_read_fw_status
[ 13.953582] TP3 wlan_sdio_read_fw_status
[ 14.060577] TP3 wlan_sdio_read_fw_status
[ 14.167562] TP3 wlan_sdio_read_fw_status
[ 14.274669] TP3 wlan_sdio_read_fw_status
[ 14.381599] TP3 wlan_sdio_read_fw_status
[ 14.488605] TP3 wlan_sdio_read_fw_status
[ 14.595582] TP3 wlan_sdio_read_fw_status
[ 14.702626] TP3 wlan_sdio_read_fw_status
[ 14.809631] TP3 wlan_sdio_read_fw_status
[ 14.916622] TP3 wlan_sdio_read_fw_status
[ 15.023626] TP3 wlan_sdio_read_fw_status
[ 15.130662] TP3 wlan_sdio_read_fw_status
[ 15.237671] TP3 wlan_sdio_read_fw_status
[ 15.344662] TP3 wlan_sdio_read_fw_status
[ 15.451687] TP3 wlan_sdio_read_fw_status
[ 15.558651] TP3 wlan_sdio_read_fw_status
[ 15.665684] TP3 wlan_sdio_read_fw_status
[ 15.772710] TP3 wlan_sdio_read_fw_status
[ 15.879725] TP3 wlan_sdio_read_fw_status
[ 15.986733] TP3 wlan_sdio_read_fw_status
[ 16.093735] TP3 wlan_sdio_read_fw_status
[ 16.200775] TP3 wlan_sdio_read_fw_status
[ 16.307846] TP3 wlan_sdio_read_fw_status
[ 16.414861] TP3 wlan_sdio_read_fw_status
[ 16.522595] TP3 wlan_sdio_read_fw_status
[ 16.629866] TP3 wlan_sdio_read_fw_status
[ 16.737107] TP3 wlan_sdio_read_fw_status
[ 16.844052] TP3 wlan_sdio_read_fw_status
[ 16.951052] TP3 wlan_sdio_read_fw_status
[ 17.058127] TP3 wlan_sdio_read_fw_status
[ 17.165090] TP3 wlan_sdio_read_fw_status
[ 17.272096] TP3 wlan_sdio_read_fw_status
[ 17.379110] TP3 wlan_sdio_read_fw_status
[ 17.486096] TP3 wlan_sdio_read_fw_status
[ 17.593076] TP3 wlan_sdio_read_fw_status
[ 17.700092] TP3 wlan_sdio_read_fw_status
[ 17.793538] logd.daemon: reinit
[ 17.814045] TP3 wlan_sdio_read_fw_status
[ 17.921091] TP3 wlan_sdio_read_fw_status
[ 17.977819] update_verifier: Started with arg 1: nonencrypted
[ 17.990803] update_verifier: Booting slot 0: isSlotMarkedSuccessful=0
[ 17.997513] update_verifier: /data/ota_package/care_map.pb doesn't exist
[ 18.004282] update_verifier: Failed to parse the care map file, skipping verification
[ 18.013624] update_verifier: Deferred marking slot 0 as booted successfully.
[ 18.020919] update_verifier: Leaving update_verifier.
[ 18.028359] TP3 wlan_sdio_read_fw_status
[ 18.047618] type=1400 audit(15.808:5): avc: denied { create } for comm="kdevtmpfs" name="dm-9" scontext=u:r:kernel:s0 tcontext=u:object_r:device:s0 tclass=blk_file permissive=0
[ 18.064319] type=1400 audit(24.220:6): avc: denied { setattr } for comm="init" name="wifi" dev="dm-9" ino=130595 scontext=u:r:vendor_init:s0 tcontext=u:object_r:wifi_data_file:s0 0
[ 18.086899] type=1400 audit(24.220:6): avc: denied { setattr } for comm="init" name="wifi" dev="dm-9" ino=130595 scontext=u:r:vendor_init:s0 tcontext=u:object_r:wifi_data_file:s0 0
[ 18.123334] type=1400 audit(24.236:7): avc: denied { search } for comm="init" name="wifi" dev="dm-9" ino=130595 scontext=u:r:vendor_init:s0 tcontext=u:object_r:wifi_data_file:s0 t0
[ 18.143230] type=1400 audit(24.236:7): avc: denied { search } for comm="init" name="wifi" dev="dm-9" ino=130595 scontext=u:r:vendor_init:s0 tcontext=u:object_r:wifi_data_file:s0 t0
[ 18.157129] TP3 wlan_sdio_read_fw_status
[ 18.161344] type=1400 audit(24.280:8): avc: denied { setattr } for comm="init" name="dhcp" dev="dm-9" ino=130599 scontext=u:r:vendor_init:s0 tcontext=u:object_r:dhcp_data_file:s0 0
[ 18.274889] TP3 wlan_sdio_read_fw_status
[ 18.405429] TP3 wlan_sdio_read_fw_status
[ 18.519955] TP3 wlan_sdio_read_fw_status
[ 18.629215] TP3 wlan_sdio_read_fw_status
[ 18.646534] init: Command 'setprop persist.service.bdroid.bdaddr 22:22:67:C6:69:73' action=early-boot (/vendor/etc/init/hw/init.freescale.rc:118) took 526ms and succeeded
[ 18.751044] TP3 wlan_sdio_read_fw_status
[ 18.858352] TP3 wlan_sdio_read_fw_status
[ 18.965321] TP3 wlan_sdio_read_fw_status
[ 19.075609] TP3 wlan_sdio_read_fw_status
[ 19.183187] TP3 wlan_sdio_read_fw_status
[ 19.237392] init: processing action (early-boot) from (/vendor/etc/init/hw/init.freescale.usb.rc:17)
[ 19.248812] init: Command 'mount configfs none /config' action=early-boot (/vendor/etc/init/hw/init.freescale.usb.rc:18) took 1ms and failed: mount() failed: Device or resource buy
[ 19.282443] init: Service 'exec 11 (/system/bin/bootstat --set_system_boot_reason)' (pid 292) exited with status 0
[ 19.315072] Mass Storage Function, version: 2009/09/11
[ 19.328699] LUN: removable file: (no medium)
[ 19.367644] using random self ethernet address
[ 19.372843] using random host ethernet address
[ 19.379164] TP3 wlan_sdio_read_fw_status
[ 19.403987] file system registered
[ 19.575578] init: processing action (early-boot) from (/vendor/etc/init/hw/init.freescale.imx8qxp.rc:13)
[ 19.604562] init: processing action (early-boot) from (/system/etc/init/installd.rc:5)
[ 19.644121] TP3 wlan_sdio_read_fw_status
[ 19.696100] init: processing action (boot) from (/init.rc:649)
[ 19.767242] init: Command 'chown radio system /sys/android_power/state' action=boot (/init.rc:691) took 52ms and failed: lchown() failed: No such file or directory
[ 19.813331] TP3 wlan_sdio_read_fw_status
[ 19.826854] init: starting service 'hidl_memory'...
[ 19.858607] init: starting service 'system_suspend'...
[ 20.429180] TP3 wlan_sdio_read_fw_status
[ 20.500869] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 20.923402] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
mek_8q:/ $ [ 21.590300] TP3 wlan_sdio_read_fw_status
[ 22.481015] TP3 wlan_sdio_read_fw_status
[ 22.501217] [VPU Encoder] enable mu for core[0]
[ 22.520188] [VPU Encoder] vpu encoder core[0] firmware version is 1.3.0
[ 23.298407] TP3 wlan_sdio_read_fw_status
[ 23.569335] read descriptors
[ 23.598477] read strings
[ 24.032127]
[ 25.189531] type=1400 audit(24.280:9): avc: denied { setattr } for comm="init" name="dhcp" dev="dm-9" ino=130599 scontext=u:r:vendor_init:s0 tcontext=u:object_r:dhcp_data_file:s0 0
[ 25.420402] type=1400 audit(31.364:10): avc: denied { read } for comm="HwBinder:309_1" name="u:object_r:default_prop:s0" dev="tmpfs" ino=226 scontext=u:r:hal_graphics_composer_def0
[ 26.577793] TP3 wlan_check_fw_status && POLL NO = 100
[ 26.971096] Fail to poll firmware status: firmwarestat=0xf005
[ 26.986997] FW failed to be active in time!
[ 26.998671] WLAN: Fail download FW with nowwait: 0
[ 27.015234] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00
[ 27.031762] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00
[ 27.047275] SDIO Func1: (0x8) 00 (0x58) 00 (0x5c) 0d (0x5d) 00 (0x60) 01 (0x61) 00 (0x62) 00 (0x64) 10 (0x65) 01 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00
[ 27.081837] SDIO Func1 (0x90-0x9a): 05 f0 00 00 00 00 00 00 00 00 00
[ 27.369748] SDIO Func1 (0x90-0x9a): 05 f0 00 00 00 00 00 00 00 00 00
[ 27.377015] woal_request_fw failed
[ 27.380685] Firmware Init Failed
[ 27.386684] woal_add_card failed
[ 27.419157] wlan_sdio: probe of mmc0:0001:1 failed with error -1
[ 27.466730] wlan: Driver loaded successfully
[ 27.554678] init: Received control message 'start' for 'bootanim' from pid: 327 (/system/bin/surfaceflinger)
[ 27.566630] init: starting service 'bootanim'...
[ 27.737183] init: Service 'early_init_sh' (pid 193) exited with status 0

 

 

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数