88W8801 RTOS Wi Fi Direct

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

88W8801 RTOS Wi Fi Direct

634件の閲覧回数
K_Sumi
Contributor I

Hi

I want to use Wi-Fi Direct with EVK-MIMXRT685 + 88W8801 + RTOS.
There is 5.22 Wi-Fi Direct in "WLAN Subsystem Host Driver-Firmware Interface". However, EVK-MIMXRT685 MCUXpresso SDK 2.14.0 does not have Wi-Fi Direct implementation. Does this mean that Wi-Fi Direct is not supported by EVK-MIMXRT685?

If there is another host board that supports 88W8801 + RTOS + Wi-Fi Direct, please let me know.

0 件の賞賛
返信
3 返答(返信)

606件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you in advance for contacting NXP support.

It is correct Wi-Fi direct is supported on all of the chipsets (88W8801), but only on Linux or Android.

We currently do not have support for Wi-Fi Direct in RTOS.

Please let me know if there is anything else where I can help you.

0 件の賞賛
返信

594件の閲覧回数
K_Sumi
Contributor I
Thanks, I understand that it is not supported on RTOS.
0 件の賞賛
返信

616件の閲覧回数
K_Sumi
Contributor I

I checked EVK-MIMXRT685 MCUXpresso SDK 2.14.0 again, but there is no Wi-Fi Direct implementation.
We have confirmed that Wi-Fi Direct is implemented in the 88W8801 WLAN driver on Linux.
From these implementations, I realized that RTOS does not support Wi-Fi Direct, but Linux does, but is this correct?

0 件の賞賛
返信