Our customer is evaluating RF characteristics using FRDM-MKW24.
Regarding Tx max power, they have one question.
The spec of max tx power is +8dBm and I could verify the power using TWR-KW24d512 before.
They observed tx power with tx un-modulated cnt transmission and informed that the power was about +2dBm.
That is to say, "Power 31" in Connectivity_Test means to +2dBm.
I feel that it is small...
Would you comment regarding the spec of the max tx power on FRDM-MKW24?
Regards,
Koichi
Hello Koichi,
I know that this is a basic question but just to be sure, could you please confirm that your customer has the correct configuration with the capacitor that selects between the SMA connector and the F antenna?
I will be looking forward for your response.
Best regards,
Earl Ramírez.
Hello Earl,
Thank you for your prompt response.
According to your comment, I confirmed to have only capacitance to SMA connector.
Regards,
Koichi
Hello Koichi,
I consulted our hardware expert and he explained me that it is an expected behavior. Let me explain why. The TWR-KW24D512 board has a better performance because the FRDM-KW24D512 has modifications in the harmonic trap to attenuate the output power in order to be candidate to obtain a certification. If you want to have a better performance you could use the same component values that the TWR-KW24D512 at the expense of lose this certification. The next revision of this board has modifications on this to achieve a better performance.
Best regards,
Earl Ramírez.
Hello Earl,
Thank you for your response.
OK.
I will inform our customer of your comment.
Regards,
Koichi