Vybrid Rev1.1 Waffle Pack Date/Lot Codes ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid Rev1.1 Waffle Pack Date/Lot Codes ?

ソリューションへジャンプ
2,350件の閲覧回数
ChrisNielsen
Contributor III

Would it be possible to confirm that the following date/lot codes are Rev1.1 silicon?: (the text below is from the label on the shrink wrapped foil enclosing the waffle pack)

Waffle Pack #1:

(1P) MPN: PVF61NN151CMK50

(1T) LOT: WD000C7300

(9D) DTE: 1309

(Q) QTY: 5

Diffused in: US

Assem in: TAIWAN(TI)

MS Level: 3, Hours: 168

Sealed: 12Jun13, Temp: 260C

PbFree=Y, RoHS=Y

2nd lvl Intct = e1

(X) LPN: RU00009FAM

Waffle Pack #2:

(1P) MPN: PVF61NS151CMK50

(1T) LOT: WD000C7900

(9D) DTE: 1309

(Q) QTY: 5

Diffused in: US

Assem in: TAIWAN(TI)

MS Level: 3, Hours: 168

Sealed: 12Jun13, Temp: 260C

PbFree=Y, RoHS=Y

2nd lvl Intct = e1

(X) LPN: RU00009FAO

I could have opended the package and inspected the part marking on the chip top but I'd prefer not to disturb the humidity controlled bag since the parts may not be soldered for several weeks.

Pictures of the labels are attached.  Thanks, Chris

ラベル(3)
0 件の賞賛
返信
1 解決策
2,022件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Since they were packed in mid June, I'd be very confident they are 1.1 silicon. Once you open them, they'll be marked with 1N02G

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,023件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Since they were packed in mid June, I'd be very confident they are 1.1 silicon. Once you open them, they'll be marked with 1N02G

0 件の賞賛
返信