Some documents needed for a non-profit students' "training + simple project"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some documents needed for a non-profit students' "training + simple project"

1,726件の閲覧回数
mohamedtaha
Contributor I

Hi,

I'm going to hold a training for students a bout DSP. It will include concepts like SIMD, VLIW, Fixed point, ...etc concepts. I was searching for an example to be used in this training and I found that SC3850 DSP is suitable. Also I studied it well in my work. SC3850 is a strong DSP which includes a lot of concepts to be discussed with students.

In order to use SC3850 as in example for the training I need the following documents:

  1. "StarCore DSP SC3850 Core Reference Manual"
  2. "C/C++ Compiler Intrinsic Functions Reference Manual" for SC3850

What are the steps should I do to use these documents in the training ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,409件の閲覧回数
andymastronardi
NXP Employee
NXP Employee

I inquired as to what you needed to do to use the documentation and there is nothing you need to do.  You can simply use the material.

Andy

0 件の賞賛
返信