Some documents needed for a non-profit students' "training + simple project"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some documents needed for a non-profit students' "training + simple project"

1,723 Views
mohamedtaha
Contributor I

Hi,

I'm going to hold a training for students a bout DSP. It will include concepts like SIMD, VLIW, Fixed point, ...etc concepts. I was searching for an example to be used in this training and I found that SC3850 DSP is suitable. Also I studied it well in my work. SC3850 is a strong DSP which includes a lot of concepts to be discussed with students.

In order to use SC3850 as in example for the training I need the following documents:

  1. "StarCore DSP SC3850 Core Reference Manual"
  2. "C/C++ Compiler Intrinsic Functions Reference Manual" for SC3850

What are the steps should I do to use these documents in the training ?

Labels (1)
0 Kudos
Reply
1 Reply

1,406 Views
andymastronardi
NXP Employee
NXP Employee

I inquired as to what you needed to do to use the documentation and there is nothing you need to do.  You can simply use the material.

Andy

0 Kudos
Reply