大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

标签

讨论

排序依据:
Lecture 1: Introduction and Motor Basics  This training module presented by Professor L. Umanand of CEDT, Indian Institute of Science, Bangalore provides an overview of the Freescale Cup – 2011. It introduces to the challenge describing the various components of the intelligent car tracker. Lecture 2: Pulse Width Modulation  This lecture provides an overview of Pulse Width Modulation Lecture 3: Control Design  This lecture describes controller design and PID control Lecture 4: Speed and Position  This Lecture discusses integrating your PID with sensor data Lecture 5: MPC5607B Overview  This training module provides an overview of the 32-bit Qorivva MPC5607B Processor. The course is targeted towards beginners in order to enable them to quick start the development of software on the MPC5607B.
查看全文
Instructions There are several main hardware configuration steps. Once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK60N512 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. In this case, the easiest way to do this is to actually navigate to the sample project and click on the Sample.mcp file. This will open CodeWarior 2.8. Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed)   Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. 1.     Unplug the USB cable.   2.     Look for the jumper (On the REV B Board) labeled "OSBDM_IRQ" - it is jumper 35. It will be found between the on/off switch and to the right of the the white "Lin" connectors. Remove one of the "LED Enable" jumpers for this if you don't have a   header jumper handy and put the jumper on the OSBDM_IRQ header These LED Jumpers are just above the blue potentiometer knob and marked as "J27."   3.    Reconnect the USB cable and click OK.   4.     Wait for the new firmware to download. 5.     A new dialog will appear when the process is complete.  6.    Unplug the cable, remove the jumper, return it to the location it was "borrowed from" and reconnect the cable. 7.    Then click OK.
查看全文
The TRK-MPC560xB: MPC560xB StarterTRAK (Development Kit) is a Freescale evaluation board powered by the qorivva chip. The Qorivva microcontrollers family is a set of 32 bit Power Architecture chips. Which Chip do you have? The chipset mounted on the boards for the Freescale Cup can vary. Always validate your chipset to know it's full capabilities. MPC560xB Product Information Page Difference Highlights: 5604B = 512MB Code Flash; no DMA 5606B = 1MB Code Flash; Has 16-Channel DMA 5607B = 1.5Mb Code Flash; Has 16-Channel DMA TRK-MPC5604B Hardware Setup There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. TRK-MPC5604B Hardware Setup Instructions Lectures: The Freescale Cup – Lecture 5: MPC5607B Overview Overview Slides from lecture Overview Slides from Lecture (PDF) other Lectures from the Freescale Cup Lecture Series Other Qorivva Tutorials: qorivva-blink-led qorivva-drive-dc-motor qorivva-turn-a-servo qorivva-line-scan-camera Board Tips Important Documents TRK-MPC5604B User's Manual TRK-MPC5604BQuick Reference Guide TRK-MPC5604B Schematics Reference manual External Links TRK-MPC5604B Webpage
查看全文
Instructions There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Install the included battery into the VBAT (RTC) battery holder. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK40x256 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. Open Codewarrior Navigate to File-> New ->Bareboard Project Select Kinetis K40->MK40X256VMD100 , P&E Open Source Jtag, C Language, No Rapid Application Development ,Finish Click on the main.c To get project focus Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed) Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. Unplug the USB cable. Look for the two pins labeled JM60 Boot and put a jumper on those pins Note: As it comes from the factory, the K40 board has a free jumper on the board. . Jumper J13 is labeled "JM60 BOOT." It connects two header pins which set the evaluation board in the firmware programming mode. This jumper is behind the LCD screen, and right next to LED/Touch Sensor "E3". Remove the LCD creen to gain access to the jumper. Reconnect the USB cable and click OK. Wait for the new firmware to download. A new dialog will appear when the process is complete. Unplug the cable, remove the jumper, and reconnect the cable. Then click OK. (You can store the jumper on the board, just set it so that it does not connect pins.) You may or may not encounter the firmware issue, or the multiple configurations issue. Once resolved, you should not see them again. With propertly set up hardware, users can return to Step 3: Import the LED Project of the Blink a LED on Kinetis Tutorial
查看全文
The Tower System is a simple concept. Take basic hardware modules, connect them together and start designing. There are two types of hardware modules, MCU/MPU and peripheral (i.e. serial, memory, LCD, etc.), which plug into backplane "elevator" boards. The Tower System supports up to four prototyping boards. The boards are installed into one of the slots in the Tower System, the signals from each installed module are shared between modules and made easily accessible through exterior headers on the Tower System. For an overview of the Tower System and some of the available modules for use, read the fact sheet here. Notes The Tower System has a "Primary" and a "Secondary" side. Most of the Tower Modules only send signals through the primary side. Many of the signals within your chip are not brought out to the tower pins. During the Hardware design process, be careful of this fact. Most often people plug the USB directly into the module, instead of using the tower USB port. You can use the Tower System modules without the tower. Designing your own Tower Module: Due to the common PCI Express standard pinouts for the tower connector, it is easy to fabricate your own tower module. See the external links section for examples. Important Documents Tower System Data Sheet Rev. 4, 5/2000 Tower Mechanical Drawing Tower System Schematics External Links Tower System Freescale Webpage Tower Geeks Website
查看全文
The TWR-K40X256 Kit is a Freescale evaluation board powered by the Kinetis K40 microcontroller. The Kinetis microcontroller family is a set of 32 bit ARM Cortex M4 chips which feature flexible storage, lower power usage, high performance and optional Floating Point Unit with many useful peripherals. For more information on the Kinetis family see Freescale's Kinetis website. The Tower System is a prototyping platform with interchangeable and reusable modules along with open source design files. Freescale K40 MCU Tower Module: TWR K40X256 Hardware Setup There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. TWR K40X246 Hardware Setup Instructions Board Specific Tutorials K40 Blink LED K40 Drive DC Motor K40 Drive Servo Motor K40 Line Scan Camera Board Tips The TWR-K40X256 features a socket that can accept a variety of different Tower Plug-in modules featuring sensors, RF transceivers, and more. The General Purpose TWRPI socket provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Table 3 of the TWR-K40X256 User's Manual, but the user manual does not describe how to order a connector. A Samtec connector, part number: SFC-110-T2-L-D-A is the proper female mating connector for the TWR-K40X256 TWRPI socket. SIDE A/SIDE B White DOTS for counting Pins Solder Wire to GND, and to MCU VDD Pin for testing purposes Important Documents TWR-K40X256 User's Manual TWR-K40X256 Schematics External Links TWR-K40X256-KIT Webpage Kinetis Discussion Forum Tower Geeks Community Website Tower Geeks Freescale Cup Group
查看全文
http://www.gpdealera.com/cgi-bin/wgainf100p.pgm?I=FUTM0043  This is the Futaba Standard Size Ball Bearing High Torque Servo. This servo can produce high-current draw from your batteries. If using NiMH or LiPo batteries, make sure they are capable of delivering approximately 2A for each servo. FEATURES: Ideal for high-torque applications requiring a standard size servo Universal connector fits Futaba, Hitec, JR, KO Propo, Airtronics Z, and Tower Hobbies. Does not fit old Airtronics A plug w/out adapter Nylon gears One bearing pre-mounted on output shaft. INCLUDES: One Futaba standard size high torque servo with; One 1.4" (35mm) diameter round servo wheel One 1.5" (39mm) diameter 4 point servo wheel One 1.25" (32mm) diameter 6 point servo wheel Four 2mm x 11mm phillips screws Four rubber grommets & Four metal eyelets REQUIRES: Small phillips screwdriver to mount to surface SPECS: Speed: 0.20 sec/60° @ 4.8V 0.16 sec/60° @ 6.0V Torque: 72 oz-in (5.2 kg-cm) @ 4.8V and 90 oz-in (6.5 kg-cm) @ 6V Dimensions: 1.6 x 0.8 x 1.5" (1-9/16 x 13/16 x 1-1/2") (40 x 20 x 38mm) Weight: 1.5oz (1-7/16oz) (41g)
查看全文
There are several programs on the market which are freely available. Below is a list of the more popular [free] ones.  Eagle PCB 123
查看全文
Below is one example process of creating a PCB. Create a Bill of Materials (BOM) In other words, decide which devices you want to use and what you will need to construct your circuit. If space is a constraint, picking the right device package is crucial. Create a Pin List Once you have all your devices. Create a simple Excel sheet of the various pin-outs from each of these devices. The goal here is to create a reference of which pin goes to which. This will greatly increase your accuracy in the next step… Create a Schematic You will need to download and install a schematic-and-layout-program. Using your schematic program create any needed device libraries and then create the schematic for the board. Create a Layout Once your done with the schematic, layout is just routing the traces around the PCB as efficiently as possible. Some tips for good routing. Use a ground plane (aka solid fill) - This helps with transient signals, and reduces trace congestion. Keep any noisy signals away from data signals (keep the motor driving lines away from data lines) Generate Gerbers and Drill Files Read the website of the Manufacturer that will be building your boards. Most of them do a good job of explaining what format the design needs to be in for them to do the job correctly. Some manufactures support the layout files from certain software toolsets (usually their own). Gerbers are pretty much the universal language though. Send to Board Manufacturer and order your BOM. Below are some of the most popular ones in the USA. If you have a resource in your area please add to the list below. pcbexpress.com sunstonecircuits.com Related Links Training by Freescale on Effective PCB Design General PCB design Engineering Articles from Quick-teck PCBs
查看全文
'''Topics we want to cover''' Advanced Components Accelerometer Gyro Ultra-sonic Temperature Humidity Pressure GPS Power Efficiency Modes Serial I/O SD Card Terminal Debugger Bluetooth Wifi RF - Zigbee Capacitive Touch Memory Data Logging Graphics Segmented Display TFT DSP CMSIS A/D conversion Advanced Motor Control Three Phase Motor Control Motor Synchronization
查看全文
Overview An H-Bridge circuit has a control circuit, usually PWM, which then determines the switching of high-voltage supply to drive a current. Typical embedded H-Bridges can drive about 5A of current. In the case, of the Freescale Cup car the motors can sustain much more current resulting in more toque and faster speeds. Performance Tuning Tips 1. You can place H-Bridges in parallel to balance the current load. For example, if you place two 5A (peak) H-Bridge outputs in parallel, the system can support up to 10A current. 2. Keep it Cool. H-Bridge's dissipate A LOT of heat. Heat = increases inefficiency of a semiconductor, so the better job you do keeping it cool, the better (and longer) it will work for you. Operation Theory This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. H-Bridge States
查看全文
How does a DC Motor work? The DC motor is a machine that transforms electric energy into mechanical energy in form of rotation. Its movement is produced by the physical behavior of electromagnetism. DC motors have inductors inside, which produce the magnetic field used to generate movement. But how does this magnetic field changes if DC current is being used? An electromagnet, which is a piece of iron wrapped with a wire coil that has voltage applied in its terminals. If two fixed magnets are added in both sides of this electromagnet, the repulsive and attractive forces will produce a torque. Then, there are two problems to solve: feeding the current to the rotating electromagnet without the wires getting twisted, and changing the direction of the current at the appropriate time. Both of these problems are solved using two devices: a split-ring commutator, and a pair of brushes. As it can be seen, the commutator has two segments which are connected to each terminal of the electromagnet, besides the two arrows are the brushes which apply electric current to the rotary electromagnet. In real DC motors it can be found three slots instead of two and two brushes. This way, as the electromagnet is moving its polarity is changing and the shaft may keep rotating. Even if it is simple and sounds that it will work great there are some issues which make these motors energy inefficient and mechanically unstable, the principal problem is due to the timing between each polarity inversion. Since polarity in the electromagnet is changed mechanically, at some velocities polarity is changing too soon, which result in reverse impulses and sometimes in changing too late, generating instantaneous “stops” in rotation. Whatever the case, these issues produce current peaks and mechanical instability. How a DC motor can be controlled? DC motors have only two terminals. If you apply a voltage to these terminals the motor will run, if you invert the terminals position the motor will change its direction. If the motor is running and you suddenly disconnect both terminals the motor will keep rotating but slowing down until stopping. Finally if the motor is running and you suddenly short-circuit both terminals the motor will stop. So there is not a third wire to control a DC motor, but knowing the previous behaviors it can be designed a way to control it, and the solution is an H-bridge. Look at the last evolution of the DC Motor above, you can observe that there are four gates and a motor connected between them. This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. Things to Consider When Using Motors With the Motor and Line scan Camera hooked up to the same board there is a significant problem with noise. The higher you turn the PWM on your drive motors the noise produced and the worse the data will appear from the camera. TO significantly reduce this noise you can simply solder an inductor directly across the 2 drive motors. This will allow you to increase the speed of the car without significantly affecting the data you receive back from the camera.
查看全文
32-bit Kinetis MCUs represent the most scalable portfolio of ARM® Cortex™-M4 MCUs in the industry. Enabled by innovative 90nm Thin Film Storage (TFS) flash technology with unique FlexMemory (configurable embedded EEPROM), Kinetis features the latest low-power innovations and high performance, high precision mixed-signal capability. For the Freescale Cup Challenge, we have provided several tutorials, example code and projects based on the twr-k40x256-kit. This board is part of the Freescale tower-system, a modular, reusable development platform that allows engineers to quickly prototype new designs. The K40 chip is a 144 pin package with 512KB of Flash, 245Kb of Program Flash, 4KB of EEProm, and 64KB of SRAM. Important Documents: Reference Manual Besides the Reference manual and the Datasheet, the most useful document for learning to program the K40 chip is the Kinetis Peripheral Module Quick Reference Data sheet Errata External Links Freescale's Kinetis K40 Product Page
查看全文
A microcontroller includes a microprocessor (CPU) as well as a number of other components like RAM, flash and EEPROM to store your programs and constants. While a microprocessor requires external devices to control things like input/output, or timers to implement periodic tasks, and digital to analog converters, a microcontroller is all inclusive. Contrast this all-in-one approach with a typical personal computer which contains an INTEL or AMD CPU, as well as separate chips for RAM, a separate video card, a dedicated hard drive, silicon chips or PCI circuit boards to enable the processor to access USB, serial and video card signals Microcontroller pins are general purpose, whereas CPU pins are specific. This means that each pin is tied to a multiplexer which you must set to choose the particular use for the pin. For example, in a microcontroller, one pin pin might be re-purposed for the following tasks 1. The output of a timer 2. Send a signal to a motor 3. Receive an input from a sensor or analog device Basic Concepts Covered Thus far: Blink an LED - overview of GPIO and setting up the microcontroller Drive a Motor - using the Timer and PWM modules of the microcontroller Turn a Servo - More details on using timer modules and PWM to control a servo Obtain Data from the Line Scan Camera - ADC Setup and GPIO Bit Blasting to create clock and pulse signals controlling the line scan camera I2C tutorial - Using I 2 C to communicate with various sensors using the K40 Button - An overview of how to implement a simple button Additional Concepts we would like to add to the Wiki: Timer Modules PWM watchdog-timer memory
查看全文
Depending on which MCU Devlopment board you have chosen, you will need to figure out a way to mount this to the chassis. I have seen everything from cardboard, to aluminum, to wood. Below is a template complete with CAD drawings to mount the Qorivva TRK-MPC5604B board and the Motor Board onto the chassis. We use plexiglass for ours, but any other millable material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260). To attach both the processor and interface boards the simillar 5mm plastic standoffs were used. Preview (.pdf) CAD file (.dxf)
查看全文
Overview Please check your local rules to confirm allowable voltage, battery chemistry and ampere-hour as these differ by region. This article is NOT a substitute for the rules. Batteries (nor Charger) are not included in the Freescale Cup kit due to global shipping complexities. Batteries can be hazardous if not stored, used and/or disposed of properly. Battery Specifications Tamiya Connector 7.2 Volts Less than or equal to 3000mAh (Check your Rules!) NiCd or NiMH Needs to have a Tamyia connector Sources of purchase   This format battery is fairly common in the radio controlled toy industry. Start your search at any local electronics store where Radio controlled toy's are sold. Retail Sources: Radio Shack (USA) - http://www.radioshack.com/product/index.jsp?productId=4273066 Fry's (USA) - http://www.frys.com/product/6468002?site=sr:SEARCH:MAIN_RSLT_PG   Online Sources All-Battery.com http://www.all-battery.com/nicd72v2400mahhighpowerbatterypackforrccarswithtamiyaconnector.aspx http://www.all-battery.com/Tenergy7.2V3000mAhRCCarNiMHBatteryPackwithCharger-91103.aspx Europe: use Conrad online stores Conrad energy NiMH Sub-C Racingpack 7.2 V / 2400 mAh Stecksystem Tamiya-Stecker im Conrad Online Shop | 206026 (Conrad Germany but same available form other sources)
查看全文
Option #1 Camera Mount Designed by Eli Hughes of WaveNumber LLC. You can order these parts through Shapeway.com which 3D prints on demand. You can choose from all sorts of materials depending on how much you want to spend. Camera Mount Option #2 To attach the camera we found useful to prepare two metal L-shaped pieces made from aluminium. With the help of black plastic distance posts (already available in the kit) and these metal stands, you may freely change the position of the camera over the surface. You may use following files to cut the required shapes (drawing was made using the QCad program): Preview (.pdf) CAD file (.dxf)
查看全文
For details on how to use the Motors, visit theDC Motor Tutorial Images Boards before 2013 Current Board Rev. 0 Rev. 1 Technical Details Revision 1 (Schematics, design files, sample code, instructional videos) Revision 0 (Schematics) H-Bridge Specifications Freescale MC33931 Datasheet Pro Tips: #1 - Electro-Magnetic Interfence (EMI) This has been mitigated in the rev. 1 board. In many cases the dc drive motors give off much EM interference causing poor data from the camera, and decreasing the servo motor performance substantially. In most cases around a PWM value of 20-25 duty cycle at the drive motors, caused detrimental problems. This problem was remedied in two ways, (1) connecting capacitors between the motor leads, the closer to the drive motor the better; (2) There is a way to connect the camera directly to the kwikstik and bypass the motor board. #2 - Rev. 0 Board workaround to Enable Braking This has been fixed in the rev. 1 board. In order to go forward AND backwards, you have to have control over IN1 and IN2 (see table below). If you look at the schematic, you can see that IN1 is directly connected to GND. In order to enable breaking you need to lift pin 43, solder a wire to it and control it properly. Tutorials General Tutorial on the DC Motor Control Qorivva: DC Motor Tutorial Kinetis Tower: DC Motor Tutorial Design evolution of motor board prior to 2010 - Freescale Cup Cars utilized the MC33932EVB 2010~2012 - Freescale Cup teams migrated to the current Interface/Motor board featuring Dual H-Bridges [Not manufactured] Tower and Trak Compatible Interface/Motor Control Board (Design files if you want to make one!) 2013+ - FRDM-KL25Z shield
查看全文
The Freescale linescan camera is based upon the TSL1401CL sensor from TAOS Inc. Design Files Schematic & 3D Render (Courtesy of eli_hughes) Images (Lens removed) Freescale Linescan Camera Specifications 128-pixel linear image sensor (TSL1401CL) Focusable imaging lens 5-pin physical interface on PCB on .100" grid Simple three-pin MCU interface with analog pixel output Lens: 7.9mm focal length, f2.4 fixed aperture, manual focus, 12mm x 0.5mm thread Exposure Time: 267µS to 68mS Resolution: 128 pixels Built-In amplifier stage to improve white/black differentiation. The lense used on the board: Alaud Optical     8.0mm f.l. Lens w/IR filter = Part Num: AB0825C        M12x.05 Lens Holder = #9 or #10 Useful links AMS TSL1401 Product Page Line Scan Camera Use Freescale App Note: Line Scan Camera
查看全文
The Kwikstik board is a great board for use in a Freescale Cup car! This page has some videos and example code to get you up and running quickly. For novice embedded developers it is recommended you use the FRDM-KL25Z for your Freescale Cup car. Board Tips The General Purpose TWRPI socket on the Kwikstik K40 board provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Kwikstik User's Manual, but the user manual does not describe how to order a connector. Soldering and directly connecting to the pins on the socket itself is very risky and not recommended. When browsing for connectors that interface with the TWRPI sockets you have two main options. 1. The first is a surface mount chip, that is a female connector to connect with the male pins on the board. There are surface mount lead on the top of the chip which will be easier to solder to. The part number is: SFC-110-T2-L-D-A 2. The second option is a female connector which mates with the male connection on the board and is then terminated with a wire for each pin. This option can greatly simplify your wiring challenges on your car as any additional lengths or wires can easily be trimmed off. The part number is: SFSD-10-28-G-12.00-S Image of the SFSD-10-28-G-12.00-S with corresponding Kwikstik TWRPI socket. Connectors can be ordered from Samtec as samples at this website: [http://www.samtec.com/suddenservice/samples/samples.aspx] Useful Videos:   Creating a new baremetal project for a Freescale KwikStik http://www.youtube.com/watch?v=P8X079Qs7cg&feature=g-upl&context=G2f166b6AUAAAAAAADAA   Debugging a bare metal project on the Freescale Kwikstik. http://www.youtube.com/watch?v=nQhhfNJZL_o&feature=g-upl&context=G2dcfcd5AUAAAAAAAEAA   Importing projects and merging code. http://www.youtube.com/watch?v=A_h9W-QRHp8&feature=g-upl&context=G2354416AUAAAAAAACAA   A discussion of the header files (and how to use them!) for Kinetis Devices in Codewarrior V10. This is the first of 2 videos. I had to split them up as I cannot upload videos greater than 15 minutes in length. http://www.youtube.com/watch?v=EP2FydCX9tY&feature=g-upl&context=G2fdf3fcAUAAAAAAABAA   Second part of the Kinetis Header file discussion http://www.youtube.com/watch?v=ygjx-OkJuS4&feature=g-upl&context=G2792e97AUAAAAAAAAAA   Discussion on getting the Clock setup on the Kwikstik http://www.youtube.com/watch?v=_FQzXhLDP2w&feature=youtu.be   How to setup GPIO on the Kinetis. Includes discussion on enabled clocks to peripherals and setting up the pin control registers. http://www.youtube.com/watch?v=GXjRpsGJJt4&feature=youtu.be   How to use the SysTick peripheral in the Cortex core with interrupts http://youtu.be/8SRqlDkJwGU   Discussion of how to setup interrupts on the NVIC. The Flex timer is used as an example http://www.youtube.com/watch?v=_mClHzxm0Wk&feature=youtu.be   Example Programs: All of the programs are bare metal examples for CodeWarrior 10.1 that can be used on the Kwikstik board. Make sure to read all of the comments in the C files! How to Load Programs In CodeWarrior: Copy only the source files and header files into a new folder. Import that new folder into CodeWarrior to avoid debug problems.   ClockSetup - Systick This example will demonstrates how to enable the 4MHz Crystal on the Kwikstik. Early versions of the Kinetis silicon had bug in which the device could crash if the clock dividers are changed while executing from FLASH (errata e2448). This code places clock initialization code in RAM. The clock code is based upon routines from Kinetis Peripheral Module Quick Reference (Freescale document KQRUG.pdf). It also shows how to enable the SysTick module in the Cortex Core. The SysTick is used to provide a delay Function. ClockSetup - SysTick.zip     FlexTimer_NVIC_IRQ This code shows how to use the NVIC in the Cortex Core. The Flex Timer module is used to generate a periodic interrupt (similar to the SysTick example). FlexTimer_NVIC_IRQ.zip   LCD_Example This code will turn on segments on the LCD on the Kwikstik. The LCD driver code is derived from the MQX based example on the Kwikstik page. LCD_Example.zip   PWM_Test This code shows how to setup the flex timers to generate different styles of PWM. Note: One of the examples sets up the flex timer for pseudo-complementary PWM. It DOES NOT use the hardware based complementary mode. It writes 2 individual registers in a software routine. One should use this a starting point to enable full hardware based complementary mode. PWM_Test.zip   CameraTest This example is a basic example on how to interface to the Freescale Linescan Camera. It will display a rough approximation of the output on the LCD. CameraTest.zip Note: The code does not run with the camera by default. This is because the AOUT is set to the pin with the pull up resistor (J15 pin 4). Once changed it will work smoothly.
查看全文