T4240 couldn't be programmed by JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 couldn't be programmed by JTAG

1,797件の閲覧回数
zhangkun2015
Contributor I

Hello,

We made a board with reference of T4240RDB, recently we met a problem which is shown in the title. After many checks,

we found an abnormal phenomenon:

  1. the impedance between VDD_OVDD_P1V8 and GND is only 9.2 Ohm,while the impedance between P1V8_AVDD and GND is 2262Ohm.
  2. 1219_4.jpg
  3. 1219_3.jpg
  4. Is there something wrong with the inner part of T4240?
ラベル(1)
タグ(1)
0 件の賞賛
12 返答(返信)

1,436件の閲覧回数
ufedor
NXP Employee
NXP Employee

The impedance in question is not characterized, so it is not specified what is its normal value.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

ufedor‌             

Hi,I need your help.Thanks a lot.

0 件の賞賛

1,436件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please confirm whether the processor is capable to complete its POR sequence - refer to the T4240 RM, 4.6.1 Power-on reset sequence.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

Thank you for your reply. But Why the impedance between VDD_OVDD_P1V8 and GND is so low?

0 件の賞賛

1,436件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics as PDF.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

Hi,thank you for your reply.

I am a fresher here. How Can I upload the PDF file ?

0 件の賞賛

1,436件の閲覧回数
ufedor
NXP Employee
NXP Employee

Just attach it to response.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

 Oh, thank you for your remind. 

 I choose the pages of the processor connections  from the schematic,and made them to PDF files.

0 件の賞賛

1,436件の閲覧回数
ufedor
NXP Employee
NXP Employee

Now please describe the processor behaviour and restate the question.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

And the second  abnormal state is :

The 1st foot of JTAG connector is short circuit.

J2.bmp

      and the net of  the 1st foot, named "COP_TDO" is directly connected to T4240's pin,which is K42.

Now, we are so worried that there is something wrong with the inside of the T4240.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

OK, the PDF is attached here.

0 件の賞賛

1,436件の閲覧回数
zhangkun2015
Contributor I

OK,Let me state the problem from the beginning.

Actually, last week, my board had just been ready for the frist time programme. But the first time we connected the debug device to the board, the problem happened. The figure is shown below.

ERROR.bmp

OK, the Chinese characters could be ignored. So, we began to check the relevant hardware.

Finally,we found two abnormal states.

  1.     the impedance between VDD_OVDD_P1V8 and GND is only 9.2 Ohm,while the impedance between P1V8_AVDD and GND is 2262Ohm.  the net of VDD_OVDD_P1V8 is only connected to two places,one is in PDF 24 and the other is in PDF 36
0 件の賞賛