T4080 DDR Memory Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4080 DDR Memory Configuration

ソリューションへジャンプ
1,728件の閲覧回数
johnmion
Contributor I

The reference manual states that  "mixing different memory types or unbuffered and registered
DIMMs in the same system is not supported". Does this include using a single-rank and dual-rank module (each one controlled by a different memory controller on the same processor)?

ラベル(1)
1 解決策
1,482件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, it does.

I would note that the problem of "mixing different memory types" is around memory interleaving. If you are not going to use interleaving between memory controllers, then you can mix different memory types between controllers, for example to use UDIMMs on one memory controller, and RDIMMs on the other one. If interleaving is required, then configurations of the memory controllers should be identical.

Regards,

Bulat

元の投稿で解決策を見る

1 返信
1,483件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, it does.

I would note that the problem of "mixing different memory types" is around memory interleaving. If you are not going to use interleaving between memory controllers, then you can mix different memory types between controllers, for example to use UDIMMs on one memory controller, and RDIMMs on the other one. If interleaving is required, then configurations of the memory controllers should be identical.

Regards,

Bulat