T1024 and T4240 are foot print compatible or not

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1024 and T4240 are foot print compatible or not

527 次查看
kamlendrachandr
Contributor I

T1024 and T4240 are foot print compatible or not

0 项奖励
回复
1 回复

442 次查看
alexander_yakov
NXP Employee
NXP Employee

No, these devices are not pin compatible, they have different number of pins - 780 pins for T1024 and 1932 pins for T4240.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复