T1024 and T4240 are foot print compatible or not

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 and T4240 are foot print compatible or not

502件の閲覧回数
kamlendrachandr
Contributor I

T1024 and T4240 are foot print compatible or not

ラベル(3)
0 件の賞賛
返信
1 返信

417件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

No, these devices are not pin compatible, they have different number of pins - 780 pins for T1024 and 1932 pins for T4240.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信