SerDes Protocol assignment to lane 4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SerDes Protocol assignment to lane 4

868件の閲覧回数
faizmajeed
Contributor III

HI!

I am using T1042 and in SerDes i select 0x08 mode. In which i can use 1 x4 PCIe , 3 x1 PCIe and 2 SATA. But i also want to use Aurora at lane 4 instead of x1 PCIe. is it possible. Please suggest some solution.

Thank You

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

775件の閲覧回数
ufedor
NXP Employee
NXP Employee

All supported SerDes protocols are explicitly shown in the processor's RM.

0 件の賞賛
返信