Dear NXP,
I am working on T4240RDB-64B machine. I needs to add the driver kernel configuration. I am using QORIQ-SDK-2.0 source.
Which defconfig do I needs to take to enable the drivers ?
Let me know the steps for build kernel with custom+default kernel configuration.
Thanks & Regards,
VinothS,
已解决! 转到解答。
You'll find which defconfig file you are using by default under sources/meta-freescale/configs/(your_machine.conf) file. For example mine is t1042d4rdb-64b.conf. And the lines inside it describes the defconfig file.
KERNEL_DEVICETREE ?= "t1042d4rdb.dtb" /* This is under arch/powerpc/dts/fsl/ folder
KERNEL_DEFCONFIG ?= "corenet64_smp_defconfig" /* This is under arch/powerpc/configs/ folder */
You can change these lines but when you repack your kernel, the new names you gave must be under the directories I mentioned in comment lines. You can have a copy of your new kernel .config. Just give it a long name while saving (vinothkumar.config). You will find that file under build directory of linux.
If you want to enable drivers exists in kernel
1) bitbake virtual/kernel -c cleansstate
2) bitbake virtual/kernel -c patch
4) bitbake virtual/kernel -c menuconfig
5) (Enable/Disable drivers you want)
6) save menuconfig with name '.config' and some other different name.
6) bitbake virtual/kernel
If you want to build out-of-tree kernel module into kernel
Take a look hello-mod recipe in poky/meta-skeleton. It includes a sample out-of-tree kernel module.
Thank You Yusuf Alriparmak
Do you know, Do we have use any defconfig from (arch/powerpc/config/85xx/ ).
And Where this .config file stored ?
Regards,
VinothS,
You'll find which defconfig file you are using by default under sources/meta-freescale/configs/(your_machine.conf) file. For example mine is t1042d4rdb-64b.conf. And the lines inside it describes the defconfig file.
KERNEL_DEVICETREE ?= "t1042d4rdb.dtb" /* This is under arch/powerpc/dts/fsl/ folder
KERNEL_DEFCONFIG ?= "corenet64_smp_defconfig" /* This is under arch/powerpc/configs/ folder */
You can change these lines but when you repack your kernel, the new names you gave must be under the directories I mentioned in comment lines. You can have a copy of your new kernel .config. Just give it a long name while saving (vinothkumar.config). You will find that file under build directory of linux.