Failed to copy __secondary_start_page

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to copy __secondary_start_page

691 Views
yixuanhao
Contributor I

Hello everyone,

   Using one customed T2080 board(DDR size 2GB,and SVR is 0x85300011 without sercurity ),plat_mp_up in U-boot,it will failed to print:

   CPU up timeout. CPU up mask is 1 should be f

    I added some print-info in u-boot as follow:

    bootpg = 0x7ffff000,pagesize = 0x1000
__bootpg_addr = 0x7fef3000,__spin_table_addr = 0x7fef3100
__second_half_boot_page = 0x3c600000,__secondary_start_page = 0x7fef2000
real CONFIG_BPTR_VIRT_ADDR = 0x7ffff000

I find a problem when the code run at memcpy((void *)CONFIG_BPTR_VIRT_ADDR, (void *)fixup, 4096) in func setup_mp.

that`s mean copy __secondary_start_page code to CONFIG_BPTR_VIRT_ADDR in my point,but i use command md to show the addr,the result as follow:

 

=> md 7ffff000

7ffff000: 00000000 00000000 00000000 00000000    ................

7ffff010: 00000000 00000000 00000000 7c7c43a6    ............||C.

7ffff020: 00000000 00000000 00000000 00000000    ................

7ffff030: 00000000 00000000 00000000 3c600001    ............<`..

7ffff040: 00000000 00000000 00000000 00000000    ................

7ffff050: 00000000 00000000 00000000 60420102    ............`B..

7ffff060: 00000000 00000000 00000000 00000000    ................

7ffff070: 00000000 00000000 00000000 4c00012c    ............L..,

7ffff080: 00000000 00000000 00000000 00000000    ................

7ffff090: 00000000 00000000 00000000 5408efbe    ............T...

7ffff0a0: 00000000 00000000 00000000 00000000    ................

7ffff0b0: 00000000 00000000 00000000 5488083c    ............T..<

7ffff0c0: 00000000 00000000 00000000 00000000    ................

7ffff0d0: 00000000 00000000 00000000 7d709ba6    ............}p..

7ffff0e0: 00000000 00000000 00000000 00000000    ................

7ffff0f0: 00000000 00000000 00000000 61ab0015    ............a...

=> md fffff000

fffff000: 00000000 00000000 00000000 00000000    ................

fffff010: 00000000 00000000 00000000 7c7c43a6    ............||C.

fffff020: 00000000 00000000 00000000 00000000    ................

fffff030: 00000000 00000000 00000000 3c600001    ............<`..

fffff040: 00000000 00000000 00000000 00000000    ................

fffff050: 00000000 00000000 00000000 60420102    ............`B..

fffff060: 00000000 00000000 00000000 00000000    ................

fffff070: 00000000 00000000 00000000 4c00012c    ............L..,

fffff080: 00000000 00000000 00000000 00000000    ................

fffff090: 00000000 00000000 00000000 5408efbe    ............T...

fffff0a0: 00000000 00000000 00000000 00000000    ................

fffff0b0: 00000000 00000000 00000000 5488083c    ............T..<

fffff0c0: 00000000 00000000 00000000 00000000    ................

fffff0d0: 00000000 00000000 00000000 7d709ba6    ............}p..

fffff0e0: 00000000 00000000 00000000 00000000    ................

fffff0f0: 00000000 00000000 00000000 61ab0015    ............a...

 

=> md 7fef2000

7fef2000: 3c608000 60630080 7c70fba6 3c600140    <`..`c..|p..<`.@

7fef2010: 60630201 7c75fba6 38600000 7c7c43a6    `c..|u..8`..||C.

7fef2020: 7c7d43a6 3c400000 60420102 7c53fba6    |}C.<@..`B..|S..

7fef2030: 7c73faa6 7c611039 4082fff8 3c600001    |s..|a.9@...<`..

7fef2040: 60630001 7c73fba6 4c00012c 7c73faa6    `c..|s..L..,|s..

7fef2050: 70610001 4182fff8 3c400000 60420102    pa..A...<@..`B..

7fef2060: 7c52fba6 7c72faa6 7c611039 4082fff8    |R..|r..|a.9@...

7fef2070: 3c600001 60630001 7c72fba6 4c00012c    <`..`c..|r..L..,

7fef2080: 7c72faa6 70610001 4182fff8 3c60ffff    |r..pa..A...<`..

7fef2090: 6063f144 80630000 7c1e42a6 5408efbe    `c.D.c..|.B.T...

7fef20a0: 540ad97e 1caa0004 7ca54214 1c850002    T..~....|.B.....

7fef20b0: 54a83032 7d434214 7c9e43a6 5488083c    T.02}CB.|.C.T..<

7fef20c0: 39080020 7d1e93a6 3da0ffff 61adf144    9.. }...=...a..D

7fef20d0: 81ad0000 55ad0026 3d601001 7d709ba6    ....U..&=`..}p..

7fef20e0: 3d60c000 616b1100 7d719ba6 65ab0000    =`..ak..}q..e...

7fef20f0: 61ab0006 7d729ba6 65ab0000 61ab0015    a...}r..e...a...

 

Obviously,the data is wrong!0x7fef2000 is address about the __secondary_start_page code data,  0x7ffff000 is real addr conver from CONFIG_BPTR_VIRT_ADDR,0xfffff000 is virt addr define in code CONFIG_BPTR_VIRT_ADDR.

I have done the thing as same in T2080RDB(DDR 4G but just use 2G, SVR is 0x85380011 with security),the result as follow: 

 

fffff000: 3c608000 60630080 7c70fba6 3c600140    <`..`c..|p..<`.@

fffff010: 60630201 7c75fba6 38600000 7c7c43a6    `c..|u..8`..||C.

fffff020: 7c7d43a6 3c400000 60420102 7c53fba6    |}C.<@..`B..|S..

fffff030: 7c73faa6 7c611039 4082fff8 3c600001    |s..|a.9@...<`..

fffff040: 60630001 7c73fba6 4c00012c 7c73faa6    `c..|s..L..,|s..

fffff050: 70610001 4182fff8 3c400000 60420102    pa..A...<@..`B..

fffff060: 7c52fba6 7c72faa6 7c611039 4082fff8    |R..|r..|a.9@...

fffff070: 3c600001 60630001 7c72fba6 4c00012c    <`..`c..|r..L..,

fffff080: 7c72faa6 70610001 4182fff8 3c60ffff    |r..pa..A...<`..

fffff090: 6063f144 80630000 7c1e42a6 5408efbe    `c.D.c..|.B.T...

fffff0a0: 540ad97e 1caa0004 7ca54214 1c850002    T..~....|.B.....

fffff0b0: 54a83032 7d434214 7c9e43a6 5488083c    T.02}CB.|.C.T..<

fffff0c0: 39080020 7d1e93a6 3da0ffff 61adf144    9.. }...=...a..D

fffff0d0: 81ad0000 55ad0026 3d601001 7d709ba6    ....U..&=`..}p..

fffff0e0: 3d60c000 616b1100 7d719ba6 65ab0000    =`..ak..}q..e...

fffff0f0: 61ab0006 7d729ba6 65ab0000 61ab0015    a...}r..e...a...

 

This data is correct!

 

I can`t understand why the data is copy wrong at,the DDR addr 0x7ffff000, i test the read-write function about 0x7ffff000~0x7fffffff is OK!

Any help is appreciated!

Labels (1)
0 Kudos
Reply
1 Reply

530 Views
Pavel
NXP Employee
NXP Employee

Test your board using the following answer in NXP Community:

https://community.nxp.com/thread/443637


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply