What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

ソリューションへジャンプ
2,443件の閲覧回数
Magnetron
Contributor III

What kind of license (Basic, Standard or Professional) I need purchase in order to get available all features (unlimited) for developing for Kinetis MCUs only?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,692件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,693件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

0 件の賞賛
返信
1,692件の閲覧回数
Magnetron
Contributor III

Anybody form Freescale Sale department can fill last line of the attached table (and win $1 :-))?

0 件の賞賛
返信
1,692件の閲覧回数
CrasyCat
Specialist III

Hello

 

I have checked with product management and indicated we are missing Kinetis specific information for the various editions.

 

Basically, special edition comes with a size limitation of 128 K. Meaning you can build ANSI C application with up to 128 K of code and data.

 

Standard edition allows to develop ANSI C application without any limitation in size ANSI C source code.

 

Professional edition allows you to develop ANSI C & C++ application without any size limitation.

 

Note that if you are using MQX OS, only the professional edition comes with support for MQX kernel awareness in the debugger.

 

I hope this helps.

 

 

CrasyCat

0 件の賞賛
返信
1,692件の閲覧回数
Magnetron
Contributor III

Thx.

0 件の賞賛
返信